Sets and reads Gain Compression Analysis controls.
These commands are Superseded by the CALCulate:MEASure:GCMeas commands.
| CALCulate:GCMeas:ANALysis | 
Click on a keyword to view the command details.
The calibration commands listed in this topic are supplemental to the Guided Cal commands.
CALC:CUSTom:DEFine - creates a gain compression measurement.
SENS:GCSetup - Most Gain Compression settings.
GC:DATA - Gain Compression data commands
Gain compression data can also be saved to a *.csv file. Learn how.
See Also
| Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Write) Enables and disables a compression analysis trace. | |
| Parameters | 
 | 
| <cnum> | Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1. | 
| <bool> | ON (or 1) - Enable compression analysis. OFF (or 0) - Disable compression analysis. | 
| Examples | CALC:GCM:ANAL:ENAB ON | 
| Query Syntax | CALCulate<cnum>:GCMeas:ANALysis:ENABle? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF | |
| Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Write) Set and return the CW frequency for a compression analysis trace. | |
| Parameters | 
 | 
| <cnum> | Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1. | 
| <num> | CW frequency in Hz. Choose a frequency within the range of the gain compression channel. | 
| Examples | CALC:GCM:ANAL:CWFR 1e9 | 
| Query Syntax | CALCulate<cnum>:GCMeas:ANALysis:CWFRequency? | 
| Return Type | Numeric | 
| Not Applicable | |
| Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Write) Sets and returns whether the CW frequency for the compression analysis trace can be set to only the discrete frequencies or provides interpolation. | |
| Parameters | 
 | 
| <cnum> | Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1. | 
| <bool> | ON (or 1) - Discrete data points only. OFF (or 0) - Interpolated data points. | 
| Examples | CALC:GCM:ANAL:ISD ON | 
| Query Syntax | CALCulate<cnum>:GCMeas:ANALysis:ISDisfrequency? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF | |
| Applicable Models: N522xB, N524xB, M9485A, E5080A (Read-Write) Sets and returns the type of data to display on the x-axis of a compression analysis trace. | |
| Parameters | 
 | 
| <cnum> | Channel number of the GCA measurement. There must be a selected measurement on that channel using Calc:Par:Sel. If unspecified, <cnum> is set to 1. | 
| <bool> | Data to display on X-axis. Choose from: 
 | 
| Examples | CALC:GCM:ANAL:XAX PIN | 
| Query Syntax | CALCulate<cnum>:GCMeas:ANALysis:XAXis? | 
| Return Type | Character | 
| PIN | |