| Meas Class | Measurement Name | Description | 
			
				| "Standard" | "S11", 
				 "S21", and 
				 so forth "A_1","A_2", 
				 and so forth | S-parameter 
				 name Unratioed parameter names with notation: "receiver_source 
				 port" See Balanced 
				 S-parameter measurement names | 
			| Active 
				 Hot Parameters | Port 
				 1 is the Source Port (DUT input). Port 3 or Port 2 can 
				 be chosen as the output of the DUT. "HotS11" "HotS31" "HotS13" "HotS33" "IPwr" "OPwr" "Gamma" "Pmax" "Xs(3,3)" "Xt(3,3)" "Xf(3,1)" "DeltaOPwr" | Learn 
				 about Active Hot parameters | 
			| "Vector 
				 Mixer/Converter" | For 
				 output port Y (input port must be 1): "S11" "VCY1" "SYY" | Learn 
				 about VMC parameters Note: Input and output 
				 ports are set up using the Mixer 
				 Setup dialog. If the ports are not 
				 set up using the Mixer Setup dialog, then ports 1 and 
				 2 are the default input and output ports and the only 
				 ports that can be used. | 
			
				| "Scalar 
				 Mixer/Converter" | For input 
				 port X and output port Y: "SCXY" "SCYX" "SXX" "SYY" "Ipwr" "RevIPwr" "Opwr" "RevOPwr" | Learn 
				 about SMC parameters Note: 
				 Input and output ports are set up using the Mixer 
				 Setup dialog. If the ports are not set up using the 
				 Mixer Setup dialog, then ports 1 and 2 are the default 
				 input and output ports and the only ports that can be 
				 used. | 
			
				| "Gain 
				 Compression" Learn 
				 more "Gain 
				 Compression Converters" Learn 
				 more | GCA and 
				 GCX: | 
			
				| "CompIn21" | Input 
				 power at the compression point. | 
			
				| "CompOut21" | Output 
				 power at the compression point. | 
			
				| "CompGain21" | Gain at the compression point. | 
			
				| "CompS11" |  Input Match at the compression 
				 point | 
			
				| "RefS21" | Linear Gain | 
			
				| "DeltaGain21" | CompGain21 -Linear Gain | 
			
				| "S11", 
				 "S21", "S12", "S22" | Standard 
				 S-parameters; measured at port 1 and port 2 | 
			
				| GCX 
				 - All Gain Compression parameters (except S21 and S12) 
				 plus the following: | 
			
				| "S11" "SC21" "SC12" "S22" "Ipwr" "RevIPwr" "Opwr" "RevOPwr" | Mixer parameters | 
			
				| "Modulation Distortion" Modulation 
				 Distortion Converters Learn 
				 more | Modulation Distortion 
				 and Modulation Distortion Converters: | 
			
				| "PIn1" | Power 
				 In | 
			
				| "POut1" | Reflected 
				 Power In | 
			
				| "POut2" | Power 
				 Out | 
			
				| "PModFile" | Power 
				 of modulation file | 
			
				| "MSig2" | Modulation 
				 Signal Out | 
			
				| "MDist2" | Modulation 
				 Distortion Out | 
			
				| "MDistIR2" | Modulation 
				 Distortion Input-referred | 
			
				| "MGain21" | Modulation 
				 Gain | 
			
				| "MComp21" | Modulation Compression | 
			
				| "PGain21" | Power Gain | 
			
				| "LMatch2" | Load match of VNA port | 
			
				| "CarrIn1" | Input Band Power | 
			
				| "CarrOut2" | Output Band Power | 
			
				| "CarrGain21" | Band Power Gain | 
			
				| "NPRIn1" | NPR at Input | 
			
				| "NPROut2" | NPR at Output | 
			
				| "NPRDist21" | NPR Distortion, Added by DUT | 
			
				| "NPRPwrIn1" | NPR Input Power | 
			
				| "NPRPwrOut2" | NPR Output Power | 
			
				| "ACPIn1" | ACP at input | 
			
				| "ACPOut2" | ACP at output | 
			
				| "ACPDist21" | ACP distortion, Added by DUT | 
			
				| "ACPPwrIn1" | ACP Input Power | 
			
				| "ACPPwrOut2" | ACP Output Power | 
			
				| "EVMDistEq21" | EVM Equalized Distortion, 
				 Added by DUT | 
			
				| "EVMDistUn21" | EVM Unequalized Distortion, 
				 Added by DUT | 
			
				| "EVMPwrIn1" | EVM Input Power | 
			
				| "EVMPwrOut2" | EVM Output Power | 
			
				| "ModFilter" | Measurement Modulation Filter | 
			
				| "A", 
				 "b1" | Port 1 test port receiver | 
			
				| "B", 
				 "b2" | Port 2 test port receiver | 
			
				| "C", 
				 "b3" | Port 3 test port receiver | 
			
				| "D", 
				 "b4" | Port 4 test port receiver | 
			
				| "R1", 
				 "a1" | Port 1 reference receiver | 
			
				| "R2", 
				 "a2" | Port 2 reference receiver | 
			
				| "R3", 
				 "a3" | Port 3 reference receiver | 
			
				| "R4", 
				 "a4" | Port 4 reference receiver | 
			| Modulation Distortion ONLY 
				 - NOT Modulation Distortion Converters | 
			
				| "S11" | Linear Input Match | 
			
				| "S21" | Linear Gain | 
			
				| "LPIn1" | Linear Input Match | 
			
				| "LPOut1" | Linear Reflected Power In | 
			
				| "LPOut2" | Linear Power Out | 
			
				| "Noise 
				 Figure Cold Source" Learn 
				 more "Noise 
				 Figure Converters" Learn 
				 more | Noise 
				 Figure AND NFX: | 
			
				| "NF" | Noise figure | 
			
				| "ENR" | Validate noise source 
				 measurements. | 
			
				| "T-Eff" | Effective noise temperature. | 
			
				| "DUTRNP" "DUTRNPI" | DUT noise power ratio. 
				 (Noise power expressed in Kelvin divided by 290). | 
			
				| "SYSRNP" "SYSRNPI" | System noise power ratio | 
			
				| "DUTNPD" "DUTNPDI" | DUT noise power density. 
				 (Noise power expressed in dBm/Hz). | 
			
				| "SYSNPD" "SYSNPDI" | System noise power density. 
				   | 
			
				| "OvrRng"(Opt 029 Only)
 | Indication that the noise 
				 receiver is being over powered. | 
			
				| "T-Rcvr" (Opt 
				 029 Only) | Temperature reading (in 
				 Kelvin) of the noise receiver board. | 
			| Noise 
				 Figure ONLY - NOT NFX: | 
			
				| "S11", 
				 "S21", "S12", "S22" | Standard S-parameters; 
				 measured with the port1 and port2 noise switches set for 
				 noise mode. | 
			
				| "A_1","A_2" 
				 ...and so forth. | Unratioed 
				 parameters; with notation:"receiver, source port"
 | 
			
				| "GammaOpt" | Optimum 
				 Complex Reflection Coefficient | 
			
				| "Rn" | Noise 
				 Resistance | 
			
				| "NFMin" | Minimum noise figure that 
				 occurs at GammaOpt | 
			| NFX 
				 ONLY: | 
			| "S11" "SC21" "SC12" "S22" "Ipwr" "RevIPwr" "Opwr" "RevOPwr" | Mixer 
				 parameters | 
			| "ALO1"," 
				 BLO1" ...and so forth. | Test 
				 port receiver at LO1 frequency | 
			| "R1_1", 
				 "B_2" ..and so forth. | Unratioed 
				 parameters with notation: "receiver_source port" | 
			| Phase Noise Learn 
				 more |   |   | 
			| PN | Phase 
				 Noise | 
			| AM | AM 
				 Noise | 
			| "Swept IMD" "Swept IMD Converters" Learn 
				 more | There are over 150 possible 
				 Swept IMD parameters, too many to list here. Build 
				 the parameters with the Swept 
				 IMD Parameter dialog, then copy the 
				 parameter name to the remote command. The following are a few 
				 example parameters: | 
			| "PwrMainLo" | Absolute 
				 power of the Low tone at the DUT output. | 
			| "IM3" | Power 
				 of the third product relative to the average power of 
				 the f1 and f2 tones measured at the DUT output. | 
			| "OIP3" | Theoretical 
				 power level at which the third product will be the same 
				 power level as the average of the main tones at the output 
				 of the DUT. | 
			| "IM Spectrum" Learn 
				 more | "Output" | View 
				 signals OUT of the DUT and into VNA port 2 (B receiver). | 
			| "Input" | View 
				 signals IN to the DUT (R1 receiver). | 
			| "Reflection" | View 
				 signals reflected off the DUT input and back into VNA 
				 port 1 (A receiver) | 
			| "IMx 
				 Spectrum Converters" Learn 
				 more | "Output" | View 
				 signals OUT of the DUT and into VNA port 2 (B receiver) | 
			
				| "Differential 
				 I/Q" Learn 
				 more | Create custom parameters 
				 using Sens:DIQ:Par:Def, 
				 then specify your custom parameter name here. The following are default parameters: | 
			
				| "IPwrF1" "OPwrF1" "GainF1" | Input Power over F1 range Output Power over F1 range Gain over F1 range | 
			
				| "Spectrum 
				 Analyzer" Learn 
				 more | "a<n>" "b<n>" where 
				 <n> is the 
				 port number to measure "ImageReject<n>" where 
				 <n> is the image reject trace | Reference 
				 receiver Test port receiver |