Controls the Active Hot Parameters configuration.
SENSe:ACTive: | DISP: | TRACe | PMAP | INPut | OUTput | SWEep: | PHASe | POINt | POWer | STARt | STEP | STOP | TYPE | TTONe: | MODE | ABSolute | RELative |
Click on a keyword to view the command details.
Applicable Models: All products with S9x111B (Read-Write) Sets whether or not interpolation is on for display. Frequency, power, and phase X axis are supported for display. Interpolation may be applied in the trace. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<bool> |
Choose from: ON or (1) Interpolate the results OFF or (0) Do NOT interpolate the results. |
Examples |
SENS:ACTive:DISP:INT 1 sense:active:disp:interpolation off |
Query Syntax |
SENSe<ch>:ACTive:DISP:INTerpolation[:STATe]? |
Return Type |
Boolean |
OFF |
Applicable Models: All products with S9x111B (Read-Write) Set and read a fixed trace input power level. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<tnum> |
The number of the trace to set input power. If unspecified, the trace number is set to 1. |
<num> |
Input power level. The range is -10 to 0. The units are Hz, dBm, or s. |
Examples |
SENS:ACTive:DISPlay:TRACe1:IPWer 0 dBm sense:active:display:trace1:ipwer 0 dBm |
Query Syntax |
SENSe<ch>:ACTive:DISPlay:TRACe:IPWer? |
Return Type |
Numeric |
Not Applicable |
Applicable Models: All products with S9x111B (Write only) Sets the input port and output port of an Active Parameter channel. This setting is necessary only when using the limited port mapping feature. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<input> |
VNA port connected to the DUT Input. Choose from any ports with dedicated internal source. |
<output> |
VNA port connected to the DUT Output. Choose from any ports with dedicated internal source. |
Examples |
SENS:ACT:PMAP 1,3 sense2:act:pmap 1,3 |
Query Syntax |
Not Applicable |
Return Type |
Not Applicable |
1,3 |
Applicable Models: All products with S9x111B (Read only) Returns the VNA test port to be connected to the DUT input for an AHP channel. The SENS:ACT:PMAP sets this value. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
Examples |
SENS:ACT:PMAP:INP? |
Query Syntax |
SENSe:ACTive:PMAP:INPut? |
Return Type |
Numeric |
1 |
Applicable Models: All products with S9x111B (Read only) Returns the VNA test port to be connected to the DUT output for an AHP channel. The SENS:ACT:PMAP sets this value. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
Examples |
SENS:ACT:PMAP:OUT? |
Query Syntax |
SENSe:ACTive:PMAP:OUTPut? |
Return Type |
Numeric |
3 |
Applicable Models: All products with S9x111B (Read-Write) Set and read the number of phase points. For the tuning tone at the output, a phase sweep is done for each point. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Phase points. Do not exceed the max number of phase points (50). |
Examples |
SENS:ACTive:SWE:PHAS:POIN 201 sense:active:sweep:phase:point 101 |
Query Syntax |
SENSe<ch>:ACTive:SWEep:PHASe:POINt? |
Return Type |
Numeric |
8 |
Applicable Models: All products with S9x111B (Read-Write) Set and read the start power level for a 3D sweep. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Start power level in dBm. Choose a value from the min power to max power of the hardware. |
Examples |
SENS:ACTive:SWE:POW:STAR 0 sense:active:sweep:power:start 0 |
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STARt? |
Return Type |
Numeric |
-10 dBm |
Applicable Models: All products with S9x111B (Read-Write) Set and read the number of power steps for a 3D sweep. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Number of power steps. The range is 2 to 20001. |
Examples |
SENS:ACTive:SWE:POW:STEP 201 sense:active:sweep:power:step 201 |
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STEP? |
Return Type |
Numeric |
201 |
Applicable Models: All products with S9x111B (Read-Write) Set and read the stop power level for a 3D sweep. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Stop power level in dBm. Choose a value from min power to max power of the hardware. |
Examples |
SENS:ACTive:SWE:POW:STOP 0 sense:active:sweep:power:stop 0 |
Query Syntax |
SENSe<ch>:ACTive:SWEep:POWer:STOP? |
Return Type |
Numeric |
0 dBm |
Applicable Models: All products with S9x111B (Read-Write) Set and read the sweep type. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<char> |
Sweep type. Choose from:
|
Examples |
SENS:ACTive:SWE:TYPE LIN sense:active:sweep:type lin |
Query Syntax |
SENSe<ch>:ACTive:SWEep:TYPE? |
Return Type |
Character |
LIN |
Applicable Models: All products with S9x111B (Read-Write) Set and read the tuning tone mode. The tuning tone is the source at the output port to extract the X parameters. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<char> |
Tuning tone mode. Choose from:
|
Examples |
SENS:ACTive:TTON:MODE ABS sense:active:ttone:mode abs |
Query Syntax |
SENSe<ch>:ACTive:TTONe:MODE? |
Return Type |
Character |
ABSolute |
Applicable Models: All products with S9x111B (Read-Write) Set and read the absolute tone power level. |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Absolute tone power level. |
Examples |
SENS:ACTive:TTON:ABS -5 sense:active:ttone:absolute -5 |
Query Syntax |
SENSe<ch>:ACTive:TTONe:ABSolute? |
Return Type |
Numeric |
-5 dBm |
Applicable Models: All products with S9x111B (Read-Write) Set and read the tone power relative to the input power (dBc). |
|
Parameters |
|
<ch> |
Any existing active match channel. If unspecified, value is set to 1. |
<num> |
Relative tone power level. |
Examples |
SENS:ACTive:TTON:REL 10 sense:active:ttone:relative 10 |
Query Syntax |
SENSe<ch>:ACTive:TTONe:RELative? |
Return Type |
Numeric |
-15 dBc |