If using the Frequency Agile.pbp setting file in this example, with a system using an external or wideband I/Q configuration, you may have to adjust the Sample Clock Rate, Modulation Bandwidth, Arb Voltage and Arb Filter parameters.
The Frequency Agile example demonstrates using the Pulse Building application's GUI to create a frequency hopping pattern. The pattern uses three different pulse definitions and modulations. Each pulse is a trapezoidal pulse type, but created using different methods available in the Pulse Building GUI. The first pulse, CW1, is created using the Pulse Building application's built-in definition parameters for a trapezoidal pulse type. The second pulse, CW2, is created using an I/Q data text file and the third pulse, CW3, uses a custom profile definition defined in a text file. Each pattern item in the frequency agile pattern is offset in frequency and one item uses a 10 dB power scaling offset.
This example demonstrates how to:
Create three different trapezoidal pulses
Build a pattern of pulses
Use pattern parameter properties such as repeats, edge jitter, and so forth
Set pattern power level and frequency
Use the power scale function to scale the amplitude of a pulse
Use the Pulse Building application's Import function
The following procedure will guide you through the steps necessary to create the three pulses used in this example.
Run the Pulse Building application.
Save this project. Use the menu selection to save the project as Frequency Agile.pbp.
Enter the following information into the Pulse Library form:
Name: CW1. Place the mouse pointer on the New Pulse 1 pulse, click the right mouse button, select Rename, and change the pulse name to CW1.
Pulse Type: Trapezoidal
Rise Time: 30 ns
Fall Time: 30 ns
Width (100%~100%): 940 ns
Width Jitter Type: None
Jitter Deviation: 0 s
Modulation Type: None
The Pulse Library form shown below displays the parameter settings for the CW1 pulse.
Click
the New Pulse button
in the Pulse Library form.
Enter the following information into the Pulse Library form:
Name: CW2. Place the mouse pointer on the New Pulse 1 pulse, click the right mouse button, select Rename, and change the pulse name to CW2.
Pulse Type: Custom I/Q
Modulation Type: None
Click the
Import
command button. Use the Open dialog box to
navigate to the Freq Agile I/Q.txt
file. The file is located in the default Pulse Building application's
...\Samples\VB6\Frequency Agile directory.
Click the Freq Agile I/Q.txt file and select Open. The I/Q data will be imported into the IQ Data table.
Click New
pulse
in the Pulse Library form.
Enter the following information into the Pulse Library form:
Name: CW3. Place the mouse pointer on the New Pulse 1 pulse, click the left mouse button, click the right mouse button, select Rename, and change the pulse name to CW3.
Pulse Type: Custom Profile
Modulation Type:None
Click the Import command button. Use the Open dialog box to navigate to the Freq Agile Custom Profile.txt file. The file is located in the default Pulse Building application's ...\Samples\VB6\Frequency Agile directory.
Click the Freq Agile Custom Profile.txt file and select Open. The custom profile data will be imported into the Profile Data table.
There are now three pulses CW1, CW2, and CW3 stored in the Frequency Agile project's Pulse Library. This section details the steps needed to create a pattern using these three pulses.
Click the Pattern Library tab at the lower left corner of the Pulse Library form.
If New Pattern 1 is not displayed in the
Pattern Library view, click the
icon.
Rename New Pattern 1 to Frequency Agile.
Click the mouse pointer anywhere in the pattern details section of the form
Click the mouse pointer on New Pattern 1 in the patterns section of the form
Click the right mouse button
Select Rename from the menu and type in Frequency Agile
Add nine
pattern items to the Frequency Agile pattern. Click the
icon nine times.
Select CW2 for the Frequency Agile pattern item at Index 2:
Click the mouse pointer in the cell located at Index 2 and Object Name in the table
Click the down arrow in the drop-down list box of that cell
Select CW2
Select CW3 for the Frequency Agile pattern item at Index 3:
Click the mouse pointer in the cell located at Index 3 and Object Name in the table
Click the down arrow in the drop-down list box of that cell
Select CW3
Enter the parameters and information as presented in the Pattern Details form below.
Index 1 - Object Name: CW1, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: -10 MHz, Phase Offset 0 rad
Index 2 - Object Name: CW2, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 0 MHz, Phase Offset 0 rad
Index 3 - Object Name: CW3, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 10 MHz, Phase Offset 0 rad
Index 4 - Object Name: CW1, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: -10 MHz, Phase Offset 1.047 rad
Index 5 - Object Name: CW2, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 0 MHz, Phase Offset 1.047 rad
Index 6 - Object Name: CW3, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 10 MHz, Phase Offset 1.047 rad
Index 7 - Object Name: CW1, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: -10 MHz, Phase Offset 2.093 rad
Index 8 - Object Name: CW2, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 0 MHz, Phase Offset 2.093 rad
Index 9 - Object Name: CW3, Repetition Interval: 3.33 us, Repeat: 1, Edge Jitter Type: None, Deviation: 0, Power Scale: 0, Freq Offset: 10 MHz, Phase Offset 2.093 rad
Click the
Connect
to Instrument button
.
Enter TCP/IP or GPIB interface parameters for the instrument in the System Configuration wizard.
Click the Test I/Ocommand button. The Status text box in the I/O Connection form should display: Connected
If an error or timeout occurs, refer to the troubleshooting section in this Help document or VISA documentation.
Click OK.
If you do not have an analyzer, you must disable the Auto-Correction routine. Go to and remove the check mark from the Auto-Correction check box.
If you are using an analyzer, perform the following steps:
Click the
Connect
to Instrument button
.
Enter TCP/IP or GPIB interface parameters for the instrument in the System Configuration wizard.
Click the TestI/Ocommand button. The Status text box in the I/O Connection form should display: Connected
If an error or a timeout occurs, refer to the troubleshooting section in this Help document or VISA documentation.
Click OK.
Click the Download menu item at the top of the form and select Download & Play. The lower section of the form, labeled VerifySignal Result: indicates the result of the signal creation and download process.
At this point the signal, defined by the Frequency Agile pattern, is loaded in the signal generator's volatile waveform memory and the signal generator is playing the signal. You can use the analyzer to view this signal. Use the following analyzer settings:
15 GHz.
200 MHz
Set the reference level to 10 dBm
- select the softkey to view the signal.
You can save this waveform file in the signal generator's non-volatile waveform memory. When you save the waveform file, instrument state parameters configured in the Advanced settings section such as frequency and amplitude are not included. Use the signal generator's Save/Recall registers to save the signal generator's instrument state. When you want to re-load the signal and play it back:
Load the signal into volatile waveform memory.
Recall the register with the signal generator's instrument state associated with the waveform file.
A signal downloaded to the signal generator's memory has a sequence file associated with it. These sequence files are loaded into the signal generator's non-volatile memory and will remain in memory until manually removed. The Pulse Building application does not remove unused sequence files. If you delete a waveform file, delete the associated non-volatile sequence file. Unused sequence files can consume signal generator memory.