Customize the Analyzer Screen


You can customize your analyzer screen by showing or hiding the following display elements. All of these selections are made from the Response > Display menu.

See Also

Expanded display capabilities of the PNA-X

Traces, Channels, and Windows

See other 'Setup Measurements' topics

Labels

You can display different labels for traces status, Y-axis and X-axis labels.

How to display labels

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Display Setup > Customize Display....

  2. Select Labels tab.

OR

  1. Press Marker > Marker Setup > Marker Display....

  2. Select Labels tab.

  1. Right click on any window area.

  2. Click Customize Display....

  3. Select Labels tab.

Programming Commands

Labels tab Dialog Box Help

Show Labels

Trace Status

Trace status is annotated at the top of each window.

The highlighted trace number indicates Active Trace.

Click the title to select a trace.

Trace Status shows the following:

  • Trace number (Tr x). This is the trace number of the channel; NOT the window trace number which is used in many programming commands

  • Measurement parameter. This can be replaced with a custom Trace Title.

  • Format

  • Scaling factor

  • Reference level

How to show/hide Trace Status.

 

Y-axis Labels

"Y-axis Labels" - allows user to show or hide the y-axis labels. 

How to show/hide Y-axis Labels.

 

X-axis Labels

How to show/hide X-axis Labels.

 

X-axis Annotation for All Traces

 Show the X-axis annotation for all traces. (Left: Checked, Right: Unchecked)

Trace Annotation for All Traces

Select to display trace annotation for all traces. (Left: Checked, Right: Unchecked)

 

Grid & Tables

How to set VNA Grid and display tables.

Each window can display only one table at a time.

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Display Setup > Customize Display...

  2. Select Grid tab.

OR

  1. Press Marker > Marker Setup > Marker Display....

  2. Select Grid tab.

  1. Right click on any window area.

  2. Click Customize Display....

  3. Select Grid tab.

Programming Commands

Grid & Table Dialog Box Help

 

Grid Lines: Solid | Dotted - Set whether to display ALL open window grid lines in solid or dotted lines. The selected setting is shown in CAPS. Once set, new windows are created using this setting. Grid lines return to SOLID when the VNA is Preset.

Set the color of the grid using Display Colors.

How to display grid settings

 

Y-axis Divisions - Set the desired rows of Y-axis, it can shows 2 to 30.

 

Y-axis Spacing -  Select either a linear or logarithmic scale Y-axis format.

 

Show Table

 

None - Turn OFF the table.


Marker Table

You can display a table of marker settings. These settings include the:

  • Marker number

  • Marker reference (for delta measurements)

  • Frequency

  • Time and Distance (for Time Domain measurements)

  • Response

Learn more about Markers


Limit Line Table

You can display, set up, and modify a table of limit test settings. These include:

  • Type (MIN, MAX, or OFF)

  • Beginning and ending stimulus values

  • Beginning and ending response values

Learn more about Limit Lines.

 


Ripple Table

You can display, set up, and modify a table of maximum ripple limit over frequency range settings. These include:

  • Type (ON or OFF)

  • Beginning stimulus value

  • Ending stimulus value

  • Maximum ripple

Learn more about Ripple limits.

 


Segment Sweep Table

You can display, set up, and modify a table of segment sweep settings. These include:

  • State (On/Off)

  • Start and Stop frequencies

  • Number of Points

  • IF Bandwidth (if independent levels)

  • Power Level (if independent levels)

  • Sweep Time (if independent levels)

Learn more about Segment Sweep.

 


Distortion Table

You can display,set up, and modify a table of modulation distortion measurement parameters. Each row represents a measurement band. Each column represents a measurement parameter.

 

Learn more about the Distortion Table.

 


Spurious, Integrated Noise, Spot Noise Tables

You can display,set up, and modify a tables of phase noise measurement parameters.

 

Learn more about the Phase Noise.

 

 

Toolbars

You can display different toolbars to allow you to easily set up and modify measurements.

How to display Toolbars

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Display Setup > Customize Display...

  2. Select Toolbars tab.

OR

  1. Press Marker > Marker Setup > Marker Display....

  2. Select Toolbars tab.

  1. Right click on any window area.

  2. Click Customize Display....

  3. Select Toolbars tab.

Programming Commands

Toolbars Dialog Box Help

 

Show Toolbar

Note: There is also a Cal Set toolbar available for Monitoring Error Terms

Softkey

Softkey is a combination of softkeys and SoftTabs. Softkeys are automatically turned ON when one of the 'function' hardkeys is pressed. This setting allows you to turn the softkeys OFF to show more measurement space on the screen. The softkeys will reappear when another function hardkey is pressed.

 

Hardkey

These keys also known as Front Keys, perform interface operations that are equivalent to those of keys in the INSTRUMENT keys, RESPONSE keys, STIMULUS keys and UTILITY keys on the front panel of VNA. Learn more.

 

Port Extensions Toolbar

The Port Extension toolbar allows you to set Port Extensions while viewing the measurement trace. Learn more about Port Extensions.

 

Transform (Time Domain) Toolbar

The Time Domain toolbar allows you to do the following:

  • Turn Transform and Gating ON/OFF.

  • Change the Start/Stop times for both Transform and Gating.

  • More... - Launches the Time Domain Transform dialog box.

  • ? - Display the help file.

  • X - Closes the toolbar.

 

Markers Toolbar

The markers toolbar allows you to set up and modify markers. It shows:

  • Marker number

  • Stimulation value

  • Marker functions:

    • Delta

    • Max/Min

    • Start/Stop

    • Center/Span

Tip: To use the Front Panel Knob to change marker position, first click the Stimulus field of the marker toolbar and then turn the knob.

Learn more about Markers

 

Cal Set Viewer Toolbar

Learn more about Cal Set Viewer.

 

External Receiver Toolbar

 The toolbar will display two receiver combo boxes and two readouts. 

 

 Receiver Combo Boxes: 

 Default is None. All Power Sensors, DC meters, and SMUs which have Active-Show in UI selected in the External Devices Configuration dialog will be displayed.

 Select External Device... to open External Devices Configuration dialog.

Note: Any device in the list which is currently being displayed as an External Receiver Measurement Trace (PMAR) is grayed out in the list and cannot be selected for measurement using this toolbar.  Likewise, after a device has been selected for display in this toolbar, it is no longer available for selection as an External Receiver Measurement Trace (PMAR).

 

Device Readouts

  • Display the data measured by the selected external receiver.

  • Readout Update:

    • update at an approximate rate of 1 time per second

    • will not update during an active sweep to avoid changing sweep timing. This may result in readouts updating at a slower rate than 1 time per second.  

    • will update even if all channels are in hold mode.

  • Display format:

    • readout space up to 6 digits.

    • For Power Sensors: 

      • default power format is dBm. 

      • User may change the format on the setup page to W format ( the entry may display W, mW, μW or nW).

    • For DVMs measuring voltage: the entry may display V, mV, μV or nV.

    • For DVMs measuring current: the entry may display A, mA, μA or nA.

Setup...  This button opens the External Receiver Toolbar Setup dialog below.

   Show Toolbar  Check to display the toolbar. 

   Receiver  These two selections are the same as the Receiver Combo Boxes displayed on the External Receiver Toolbar.

   Average  Indicates the averaging used for the receiver measurement. The valid range is 1 to 65535. The default value is 1.

   Format   The display format as as the format of the device readouts in toolbar.

                   For the DVM or SMU, the format will display either V or A, depending on the settings configured in the External Device Properties dialog. This cannot be edited. 

   Frequency  

  • For receiver = DVM, SMU and None, the frequency will display "-". This cannot be edited. 

  • For receiver = Sensor

    • User may enter the frequency used for correcting the power measurement.

    • By default, this field displays Default and uses the default frequency value.

    • If the user enters a blank value or 0, the field automatically reverts to displaying Default and the default frequency is used.  

    •  

All Off (NOT on softkeys)

This allows you to hide all toolbars with a single selection. NOT available on sofkeys.

 


Other Bars

Main Title

The Main Title shows the title of VNA window and Minimize / Maximize icons.

  • Checked - Title bars for all VNA window are shown.

  • Cleared - Title bars for all VNA window are hidden. This allows more room to display measurement results.

Active Entry Toolbar

When used with softkeys, this area allows numeric values to be entered for settings. From the keyboard, enter G for Giga, M for Mega or milli, K for kilo and so forth.

 

Status Bar

2 Bars

When enabled, the status bar is displayed along the bottom of the VNA screen. The primary status bar shows the following:

Tip: Right-click on many of these items in the status bar for quick access to settings.

Note: A second level status bar appears when using External Test Set Control or Interface control.

The status bar state (ON or OFF) will not change when the VNA is Preset.

 

Clock (System Date and Time)

The VNA system date and time can be shown in the far right corner of the status bar.

The format is: year-month-day  hr:min and can NOT be changed.

To hide the clock, right click the mouse on the clock and then click Hide Clock.

Learn how to set the VNA time settings.

 

Active Port

Check to enable the active port feature. All VNA port numbers will be displayed in a status bar whether they are active or not. The currently active port will be highlighted in blue.

If the ports change state more quickly than 4 Hz in standard channel, all active ports will be highlighted with a constant blue color.

The location of the active port indicators depend on the state of the "2 Bars" selection, the number of VNA ports and the width of the display.

Selecting Measurement Class other than Standard will disable the Active Port Pane. If both Application and Standard measurement channels are selected, the indications for Standard channel will only be shown on the pane. 

Use-Case example:

1. "2 Bars" is OFF. The active port indicators on 2nd bar.

2.  "2 Bars" is ON. The active port indicators on 1st bar.

3. "2 Bars" is ON. The active port indicators on 3rd bar. (when number of port indicators > (Wapp-1000)/20, where Wapp is application width in pixels.)

 

Display Sheet Tabs

Top - Display sheet tabs above display.

Bottom - Display sheet tabs below display.

 

 

Tools

How to set Tools settings

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Display Setup > Customize Display...

  2. Select Tools tab.

OR

  1. Press Marker > Marker Setup > Marker Display....

  2. Select Tools tab.

  1. Right click on any window area.

  2. Click Customize Display....

  3. Select Tools tab.

Programming Commands

Tools Dialog Box Help

Tools function to create a shortcut icon to display on Active Entry or Softkey Toolbar. The maximum icons can display on Active Entry is 9, while Softkey Toolbar is 12.

New Window - Create a new window.

New Channel - Create a new channel on active window.

New Channel + Window - Create a new trace and channel to a new window.

New Trace - Create a new trace on active window.

New Trace + Window - Create a new trace to a new window, but the channel is remain.

New Sheet - Create a new sheet.

New Trace + Sheet - Create a new trace to a new sheet, but the channel is remain.

New Channel + Sheet - Create a new trace and channel to a new sheet.

Home - Display VNA Home softkeys.

Favorite - Set favorite application. To Add a Favorite, press and hold any softkey for three seconds and select the desired Favorite number (Favorite 1 to 3).

Help - Shows Help file.

Show Task Bar - Shows Window bar.

Preference - Display preference dialog box.

Tile Windows

Manages Files - Use to manage the saved files in the "D:\" drive folder. Learn more.

Minimize Application - Restore VNA screen. Learn more.

About Network Analyzer - Display About Network Analyzer dialog box.

Undo - Recover to previous version. Learn more.

Redo - Set to latest version. Learn more.

Screenshot - Save screen figure to "D:\" drive (D:\).

Delete - Delete the active window.

 

 

Colors

How to set colors

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Display Setup > Customize Display...

  2. Select Colors tab.

  1. Right click on any window area.

  2. Click Customize Display....

  3. Select Colors tab.

Programming Commands

Colors Dialog Box Help

Menu Color Theme - Select color theme

Display Colors... - See Display Colors

Print Colors... - See Print Preview

 

Window Title

You can create and display a title for each window.

How to enter a Window Title

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Display > Window Setup > Window Title....

  1. Move a cursor in the grid and then right click.

  2. Select Title....

Programming Commands

Window Title Dialog Box Help

  1. Click Enable, then type the window title. Click Keyboard to type with a mouse.

  2. To remove the window title, clear the Enable checkbox or delete the text from the dialog entry.

 

Trace Title

A Trace Title overwrites the Measurement Parameter in the Trace Status area, the Status Bar and hardcopy prints.

How to enter a Trace Title

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Trace > Trace Setup > Trace Title....

  1. Move a cursor in the grid and then right click.

  2. Select Trace Title....

Programming Commands

Trace Title Dialog Box Help

  1. Click Enable, then type the window title. Click Keyboard to type with a mouse.

  2. To remove the window title, clear the Enable checkbox or delete the text from the dialog entry.

 

Frequency/Stimulus

Frequency/stimulus information is displayed at the bottom of each window on the screen. It shows:

How to show/hide Frequency/Stimulus information


 

Minimize Application

The Network Analyzer application can be minimized to show the desktop and Windows taskbar.

  1. Click System > Main > Minimize Application.

To restore the VNA application, double-click the VNA application on the desktop.