Write-only |
About ECAL Confidence Check |
Description |
Note: This property is replaced by AcquireCalConfidenceCheckECALex Method Transfers confidence data from the specified ECal module into the measurement's memory trace. The data is transferred to the specified S-parameter on the same channel as this Calibrator object. The characterization within the ECal module that the confidence data will be read from is specified by the ECALCharacterization property on the ICalibrator2 interface. The default value of the ECALCharacterization property is naECALFactoryCharacterization. |
VB Syntax |
cal.AcquireCalConfidenceCheckECAL Sparam[,ecalModule] |
|
|
|
Variable |
(Type) - Description |
|
cal |
A Calibrator (object) |
|
Sparam |
(String) S-parameter to transfer confidence data to. This parameter must be present on the same channel as the calibrator object. |
|
ecalModule |
(enum NAECALModule) – Optional argument. ECal module. Choose from: 0 - naECALModule_A (default, if unspecified) 1 - naECALModule_B |
Return Type |
None |
Default |
Not applicable |
|
|
|
Examples |
Cal.AcquireCalConfidenceCheckECAL "S11", naECALModule_A |
|
|
|
C++ Syntax |
HRESULT AcquireCalConfidenceCheckECAL( _bstr_t strParameter, enum NAECALModule ecalModule ); |
Interface |
ICalibrator |