Write-only |
About ECAL Confidence Check |
Description |
This method replaces AcquireCalConfidenceCheckECAL Transfers confidence data from the specified ECal module into the measurement's memory trace. The data is transferred to the specified S-parameter on the same channel as this Calibrator object. The characterization within the ECal module that the confidence data will be read from is specified by ECALCharacterizationEx. The default value is 0. Note: A confidence check can NOT be performed remotely from User Characterizations that are stored on the VNA disk. |
VB Syntax |
cal.AcquireCalConfidenceCheckECALEx Sparam [,ecalModule] |
Variable |
(Type) - Description |
|
cal |
A Calibrator (object) |
|
Sparam |
(String) S-parameter to transfer confidence data to. This parameter must be present on the same channel as the calibrator object. |
|
ecalModule |
(Integer) – Optional argument. ECal module. Choose from modules 1 through 8 Use IsECALModuleFoundEx to determine the number of modules connected to the VNA Use GetECALModuleInfoEx to return the model and serial number of each module. |
Return Type |
None |
Default |
Not applicable |
Examples |
Cal.AcquireCalConfidenceCheckECALEx "S11", 2 |
C++ Syntax |
HRESULT AcquireCalConfidenceCheckECALEx(BSTR strParameter, long moduleNumber = 1); |
Interface |
ICalibrator4 |