Write-only |
About Cal Window |
Description |
Show the Cal Window, and optionally one or more other specific windows, before acquiring a Cal standard. This command will cause the Cal Window to display the specific measurements that are to be made for that particular Cal standard. |
VB Syntax |
guidedCal.SetupMeasurementsForStep (n) |
Variable |
(Type) - Description |
|
guidedCal |
A GuidedCalibration (object) |
|
n |
Step number in the calibration process. Use GenerateSteps to determine the total number of steps. Use GetStepDescription to read the description of each step. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
guidedCal.SetupMeasurementsForStep 3 |
C++ Syntax |
HRESULT SetupMeasurementsForStep(long step); |
Interface |
IGuidedCalibration4 |