File  |  Instrument  |  Response  |  Stimulus  |  Utility  |  Cal  |  Apps  |  Remote ONLY


 

Unguided | SmartCal (Guided) | ECAL | Guided Power Cal | Cal All | Save-Recall | Cal Sets | Cal Types | Prefer's |Correction | Port Ext | Fixturing | CPM | Delta Match | Cal Kits | Standards | Real-time Uncertainty | Multiple Sensors | Source Pwr Cal | Power Sensors | Receiver Cal | Cal Data | CalPod | Custom Cal Window | AFR | Cal Update

Description

SCPI

See Also: Calibration commands for Apps

COM

Perform an Unguided Calibration

Launch Cal Wizard

SYSTem:CORRection:WIZard

app.LaunchCalWizard

Set Cal Type

SENSe:CORRection:COLLect:METHod

cal.SetCalInfo

Select a Cal Kit

SENSe:CORRection:COLLect:CKIT

app.CalKitType

Get a Handle to the Active Cal Kit

None

app.ActiveCalKit

Simultaneous 2-Port Calibration

SENSe:CORRection:TSTandards

cal.Simultaneous2PortAcquisition

Acquisition Direction

SENSe:CORRection:SFORward

cal.AcquisitionDirection

Measure a Standard

SENSe:CORRection:COLLect

cal.AcquireCalStandard

Calculate Errors

SENSe:CORRection:COLLect:SAVE

cal.CalculateErrorCoeffecients

Do Isolation

SENSe:CORRection:COLLect

cal.AcquireCalStandard

Perform and apply Response (Normalization) cal

SENSe:CORRection:COLLect:METHod

DoResponseCal

 

Perform a Guided Cal

Initiate a Guided Cal

SENSe:CORRection:COLLect:GUIDed:INITiate

Initialize

List valid Connector Types for a Port

SENSe:CORRection:COLLect:GUIDed:CONNector:CATalog?

ValidConnectorTypes

List valid Cal Kits for a Connector type.

SENSe:CORRection:COLLect:GUIDed:CKIT:CATalog?

GetCompatibleCalKits

Select a Connector Type

SENSe:CORRection:COLLect:GUIDed:CONNector:PORT

ConnectorType

Select a Cal Kit

SENSe:CORRection:COLLect:GUIDed:CKIT:PORT

CalKitType

Set cal method for each port pair.

SENSe:CORRection:COLLect:GUIDed:PATH:CMEThod

PathCalMethod

Set Thru Method for each port pair.

SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod

PathThruMethod

Set Thru Port Pairs

SENSe:CORRection:COLLect:GUIDed:THRU:PORTs

ThruPortList

Return Number of Steps in a Cal

SENSe:CORRection:COLLect:GUIDed:STEPs?

GenerateSteps

Return a Description of a Cal Step

SENSe:CORRection:COLLect:GUIDed:DESCription?

GetStepDescription

Measure a Cal Standard in a Guided Cal

SENSe:CORRection:COLLect:GUIDed:STAN

AcquireStep

Save Cal

SENSe:CORRection:COLLect:GUIDed:SAVE

GenerateErrorTerms

Return Number of Steps in a Cal

SENSe:CORRection:COLLect:GUIDed:LIST:COUNt?

None

Return number of standards for step[n]

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:COUNt?

None

Return step description

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:DESCription?

None

Return label for complete standard

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:LABel?

None

Return number of ports on standard used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:PORTs?

None

Return label for one of the standards in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:LABel?

None

Return number of ports on one of the standards used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:PORTs?

None

Return the enumeration for the type of standard

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:STYPe?

None

Return list of VNA test ports to which one of the standards is attached

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STANdard:TPORts?

None

Return enumeration for the type of standard device used in the step

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:STYPe?

None

Return list of VNA test ports to which the standard(s) in this step is attached

SENSe:CORRection:COLLect:GUIDed:LIST:STEP:TPORts?

None

Return measurement parameters measured in the specified step number of a guided calibration

SENSe:CORRection:COLLect:GUIDed:DATA:CATalog?

None

Set and return measurement data for a specified measurement parameter of a particular step of a guided cal

SENSe:CORRection:COLLect:GUIDed:DATA

None

Enable/disable using existing source power calibration array when acquiring calibration standard data:

SENSe:CORRection:COLLect:GUIDed:PCAL:APPLy

None

Return list of ports being calibrated by an active calibration session

SENSe:CORRection:COLLect:GUIDed:PORTs?

None

 

Adapter settings for Unknown Thru or Adapter Removal

Sets use of a THRU adapter

SENSe:CORRection:COLLect:GUIDed:ADAPter:CREate

None

Set adapter delay

SENSe:CORRection:COLLect:GUIDed:ADAPter:DELay

None

Set adapter description

SENSe:CORRection:COLLect:GUIDed:ADAPter:DESCription

None

Set port pairs for adapter

SENSe:CORRection:COLLect:GUIDed:ADAPter:PATHs

None

Clear the settings

SENSe:CORRection:COLLect:GUIDed:ADAPter:COUNt:ZERO

None

Return number of adapters

SENSe:CORRection:COLLect:GUIDed:ADAPter:COUNt?

None

 

Optional Guided Cal commands

Auto-Orient  ECal

SENSe:CORRection:PREFerence:ECAL:ORIentation

cal.OrientECALModule

Manual orient ECAL

SENSe:CORRection:PREFerence:ECAL:PMAP

cal.ECALPortMapEx

Read orientation

SENSe:CORRection:CKIT:ECAL:ORIent?

ECalModules

Calculate Error Terms from a Guided Cal

SENSe:CORRection:COLLect:GUIDed:SAVE

GenerateErrorTerms

Save Cal to an existing Cal Set GUID

SENSe:CORRection:COLLect:GUIDed:SAVE:CSET

None

Load Eterms during a cal

SENSe:CORRection:COLLect:GUIDed:ETERms:LOAD

None

Perform Isolation

SENSe:CORRection:COLLect:GUIDed:ISOLation:PATHs

GetIsolationPaths Method

SetIsolationPaths Method

Increment Avg for Isolation

SENSe:CORRection:COLLect:GUIDed:ISOLation:AVERage:INCRement

IsolationAveragingIncrement Property

Abort Guided cal

SENSe:CORRection:COLLect:GUIDed:ABORt

None required. Destroy the GuidedCal object to terminate a cal.

Execute the Ecal calibration

SENSe:CORRection:COLLect:GUIDed:ECAL:ACQuire

None

Specifies the Ecal Kit for Ecal Calibration

SENSe:CORRection:COLLect:GUIDed:ECAL:SELect

None

Compute Error Terms

SENSe:CORRection:COLLect:GUIDed:ETERms:COMPute

None

 

Guided Power Cal

Use standard Source Power commands to make advanced settings.

Use Power Sensor commands to configure the power sensor.

Perform power cal

SENSe:CORRection:COLLect:GUIDed:PSENsor

PerformPowerCalibration

Power sensor connector type

SENSe:CORRection:COLLect:GUIDed:PSENsor:CONNector

PowerSensorConnectorType

Cal Kit for power cal

SENSe:CORRection:COLLect:GUIDed:PSENsor:CKIT

PowerSensorCalKitType

Power Level for cal

SENSe:CORRection:COLLect:GUIDed:PSENsor:POWer:LEVel

PowerCalibrationPowerLevel

Perform match-correction

SENSe:CORRection:METHods:MATCh

MatchCorrectPower

Sets and returns the selected ports to include in a full NPort correction.

SENSe:CORRection:METHods:PORT:SUBSet:FULL[:VALue]

FullyCorrectedPorts

Resets the full and response list to their default values.

SENSe:CORRection:METHods:PORT:SUBSet:RESet

ResetPortValues

Sets and returns the selected ports to be corrected with enhanced response calibration.

SENSe:CORRection:METHods:PORT:SUBSet:RESPonse[:VALue]

ResponseCorrectedPorts

Set and return the ON/OFF subset correction state.

SENSe:CORRection:METHods:PORT:SUBSet:[:STATe]

CorrectionSubsettingState

Load Power Table

SENSe:CORRection:COLLect:GUIDed:PSENsor:POWTable

 Used with SMC on mmWave systems.

PowerTableFilename

 Used with SMC on mmWave systems.

 

Perform Enhanced Response Cal

Set guided Cal method

SENSe:CORRection:COLLect:GUIDed:PATH:CMEThod

PathCalMethod

Set guided Thru method

SENSe:CORRection:COLLect:GUIDed:PATH:TMEThod

PathThruMethod

 

Perform Sliding Load Acquisition

Set preference to not prompt

SENSe:CORRection:COLLect:GUIDed:PREFerence:SLIDingload

SlidingLoadAcquisitionBehavior

Read iteration step

SENSe:CORRection:COLLect:GUIDed:ITERations:COUNt?

IterationCountForStep

Read minimum iterations

SENSe:CORRection:COLLect:GUIDed:ITERations:MINimum?

MinimumIterationsForStep

Reset iterations

SENSe:CORRection:COLLect:GUIDed:ITERations:RESet

ResetStep

 

Perform an ECAL

Specify Module and Characterization

SENSe:CORRection:COLLect:ACQuire

cal.ECALCharacterizationEx

Do ECAL 1-Port

SENSe:CORRection:COLLect:CKIT 99

cal.DoECAL1PortEx

Do ECAL 2-Port

SENSe:CORRection:COLLect:CKIT 99

cal.DoECAL2PortEx

Get ECAL Module Info

SENSe:CORRection:COLLect:CKIT:INFormation?

SENSe:CORRection:CKIT:ECAL:INFormation?

cal.GetCalKitTypeString

cal.GetECALModuleInfoEx

Get list of ECal Modules attached to PNA

SENSe:CORRection:CKIT:ECAL:LIST?

cal.ECALModuleNumberList

Get list of characterizations in ECal module

SENSe:CORRection:CKIT:ECAL:CLISt?

cal.ECALCharacterizationIndexList

Perform Module Orientation during calibration

SENSe:CORRection:PREFerence:ECAL:ORIentation

cal.OrientECALModule

Maps ECAL Module to PNA Ports

SENSe:CORRection:PREFerence:ECAL:PMAP

cal.ECALPortMapEx

Reads ECal orientation

SENSe:CORRection:CKIT:ECAL:ORIent?

ECalModules

Perform ECal Isolation

SENSe:CORRection:COLLect:ISOLation:ECAL

ECALIsolation

Increment Avg for ECal Isolation

SENSe:CORRection:COLLect:ISOLation:AVERage:INCRement

IsolationAveragingIncrement

Return the ID string of ECals

SYSTem:COMMunicate:ECAL:CATalog?

None

Return a list of characterizations

SYSTem:COMMunicate:ECAL:CLISt?

None

Return the number of installed cal kits

SYSTem:COMMunicate:ECAL:COUNt?

None

Delete user characterizations from VNA disk memory

SYSTem:COMMunicate:ECAL:DMEMory:CLEar

None

Import file into VNA disk memory

SYSTem:COMMunicate:ECAL:DMEMory:IMPort

None

Save existing ECal characterization to a file

SYSTem:COMMunicate:ECAL:EXPort

None

Read identification and characterization information for ECal module

SYSTem:COMMunicate:ECAL:INFormation?

None

Read identification and characterization information from  ECal module or VNA disk memory

SYSTem:COMMunicate:ECAL:KNAMe:INFormation?

None

Return list of index numbers for ECal modules

SYSTem:COMMunicate:ECAL:LIST?

None

Return number of unique states for specified path name on selected ECal module

SYSTem:COMMunicate:ECAL:PATH:COUNt?

None

 

Perform ECal User Characterizations

Perform User ECal Characterization

All SCPI commands

All COM commands

Manage PNA Disk Memory Characterizations

Delete disk memory characterizations.

SENSe:CORRection:CKIT:ECAL:DMEMory:CLEar

None

Saves a disk memory characterization to an archive file.

SENSe:CORRection:CKIT:ECAL:EXPort

None

Imports the ECal characterization from the specified archive file.

SENSe:CORRection:CKIT:ECAL:DMEMory:IMPort

None

Reads the user-characterization info from ECal module or PNA disk memory.

SENSe:CORRection:CKIT:ECAL:KNAMe:INFormation?

None

 

ECal Confidence Check

Confidence Check Parameter

SENSe:CORRection:CCHeck:PARameter

cal.AcquireCalConfidenceCheckECALEx

Confidence Check Acquire

SENSe:CORRection:CCHeck

cal.AcquireCalConfidenceCheckECALEx

Confidence Check Done

SENSe:CORRection:CCHeck:DONE

cal.DoneCalConfidenceCheckECAL

Set/Read ECal State

Sets the state of an ECAL module

CONTrol:ECAL:MODule:PATH:STATe

None

Read ECal state data

SENSe:CORRection:CKIT:ECAL:PATH:DATA?

None

Read number of ECal states for specified path

CONTrol:ECAL:MODule:PATH:COUNt?

SENSe:CORRection:CKIT:ECAL:PATH:COUNt?

None

 

Calibrate All Channels

Select the channels to be calibrated.

SYSTem:CALibrate:ALL:SELect

Channels

Set the IFBW

SYSTem:CALibrate:ALL:IFBW

IFBW

Set the power level

SYSTem:CALibrate:ALL:PORT:SOURce:POWer

PowerLevel

Set the power offset

SYSTem:CALibrate:ALL:PORT:SOURce:POWer:OFFSet

PowerOffset

Set the receiver atten

SYSTem:CALibrate:ALL:PORT:RECeiver:ATTen

ReceiverAttenuator

Set the source atten

SYSTem:CALibrate:ALL:PORT:SOURce:POWer:ATTen

SourceAttenuator

Set the User Calset Prefix

SYSTem:CALibrate:ALL:CSET:PREFix

UserCalsetPrefix

Set Path Configuration

SYSTem:CALibrate:ALL:PATH:CONFigure:ELEMent

PathConfigurationElement

Read unique Cal properties

SYSTem:CAL:ALL:MCLass:PROPerty:NAME:CATalog?

PropertyNames

Read unique property values

SYSTem:CAL:ALL:MCLass:PROPerty:VALue:CATalog?

PropertyValues

Set property name/value

SYSTem:CAL:ALL:MCLass:PROPerty:VALue

PropertyValue

Read primary Cal channel

SYSTem:CALibrate:ALL:GUIDed:CHANnel[:VALue]?

None

Get GuidedCal handle

None

GuidedCalibration

For each channel, sets the ports to be calibrated.

SYSTem:CALibrate:ALL:CHANnel:PORTs

CalibrationPorts

Returns a final list of ports to be calibrated.

SYSTem:CALibrate:ALL:GUIDed:PORTs?

SParameterCalPorts

Read generated Cal Sets

SYSTem:CALibrate:ALL:CSET:CATalog?

GeneratedCalsets

Returns all cal all guided calibration channels

SYSTem:CALibrate:ALL:GUIDed:CHANnel:LIST?

None

Returns available ports for independent power calibration.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:CATalog?

ValidPorts

Adds a power cal range for a specific port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:ADD

AddPowerCalRange

Resets all ranges for the given source port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:CLEar

Reset

Queries how many ranges are included in the calibration for source port <n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:COUNt?

RangeCount

Sets and gets the number of points for range <m> for source port<n>. 

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:POINts

NumberOfPoints

Sets and gets the start frequency for range <m> for source port<n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STARt

StartFrequency

Sets and gets the stop frequency for range <m> for source port<n>.

SYSTem:CALibrate:ALL:INDependent:SOURce:CALibrate:RANGe:STOP

StopFrequency

 

Recall / Save / Apply a Calibration or Error Term

Recall a Calibration

SENSe:CORRection:CSET

app.Recall

Apply a Calibration to a measurement

SENSe:CORRection:CSET

app.Recall

Save a Calibration

SENSe:CORR:CSET:SAVE

app.Save

Save or Recall an Error Term

CALCulate:DATA Scorr

Data Topic

Read/ Write Cal Set data

SENSe:CORRection:CSET:DATA

None

Apply an Error Term after Uploading

SENSe:CORRection:COLLect:APPLy

None

Cal Sets

Quickly test a prototype of automation software

SENSe:CORRection:CSET:CREate:DEFault

None

Create a Cal Set

SENSe:CORRection:CSET:CREate

calMgr.CreateCalSet

Delete a Cal Set

SENSe:CORRection:CSET:DELete

calMgr.DeleteCalSet

List Cal Sets

CSET:CATalog?

calMgr.GetCalSetCatalog

List Cal Sets in VNA

None

EnumerateCalSets

Get Cal Set Information

None

calMgr.GetCalSetUsageInfo

List Cal Set Error Terms

SENSe:CORRection:CSET:ETERM:CATalog?

Get ErrorTermList2

Return if a Cal Set exists

CSET:EXISts?

Exists

None

Select a Cal Set by GUID

SENSe:CORRection:CSET:ACTivate

calMgr.GetCalSetByGUID

Apply a Cal Set to a channel

SENSe:CORRection:CSET:ACTivate

channel.SelectCalSet

Copy a Cal Set

SENSe:CORRection:CSET:COPY

CalSet.Copy

Save a Cal Set

SENSe:CORRection:CSET:SAVE

CalSet.Save

Save Cal Sets

None

app.SaveCalSets

Automatically save to User Cal Set

SENSe:CORRection:PREFerence:CSET:SAVE

None

Change the Description of a Cal Set

SENSe:CORRection:CSET:DESCription

CalSet.Description

Change the Name of a Cal Set

SENSe:CORRection:CSET:NAME

calset.Name

Recall a Cal File

MMEMory:LOAD

app.Recall

Save 'in-memory' Cal Set to disk.

SENSe:CORRection:CSET:FLATten

None

Create Cal Set with De-embeded fixture removed.

CSET:FIXTure:DEEMbed

Deembed

Create Cal Set with Matching Network included.

CSET:FIXTure:EMBed

Embed

Adds stimulus data to a specific buffer.

None

PutErrorTermStimulus

Returns the stimulus values over which the specific error term was acquired.

None

GetErrorTermStimulus

Returns FOM stimulus values from a Calset.

SENSe:CORRection:CSET:STIMulus?

StimulusValues

Returns the Cal Types from the calset.

None

ContentDescriptor

Returns the properties of the calset.

None

Properties

Returns the numbers of the channels using the calset.

None

ChannelClients

Unselect Cal Set

SENSe:CORRection:CSET:DEACtivate

UnselectCalset

 

Cal Set Items

Returns names of the items in a cal set

SENSe:CORRection:CSET:ITEM:CAT?

Item

Remove name-value pair from cal set

None

RemoveItem

Read the value of the Cal Set item.

SENSe:CORRection:CSET:ITEM[:DATA]?

None

Enumerate name-value pair items in the cal set.

None

EnumerateItems

 

Apply Cal Types

Catalog ALL Cal Types for the PNA

SENSe:CORRection:TYPE:CATalog?

calMgr.GetCalTypes

Catalog Cal Types in the Cal Set

SENSe:CORRection:CSET:TYPE:CATalog?

None

Is a specific Cal Type contained in the Cal Set?

None

calMgr.HasCalType

Set and return the measurement Cal Type

CALCulate:MEASure:CORRection:TYPE

meas.CalibrationTypeID

Set port to measure QSOLT reflection standards.

None

None

 

Correction Settings

Turn Correction ON|OFF for a channel

SENSe:CORRection

chan.ErrorCorrection

Turn Correction ON|OFF for a measurement

CALCulate:MEASure:CORRection[:STATe]

meas.ErrorCorrection

Interpolation ON|OFF

SENSe:CORRection:INTerpolate

meas.InterpolateCorrection

Returns the error correction state for the measurement

CALCulate:MEASure:CORRection:INDicator?

ErrorCorrectionIndicator

 

Preferences

Set default  Cal Set Save behavior

SENSe:CORRection:PREFerence:CSET:SAVE

RemoteCalStoragePreference

Sets behavior for simulated cal

SENSe:CORRection:PREFerence:SIMCal

None

External or internal trigger during cal

SENSe:CORRection:PREFerence:TRIG:FREE

PreferInternalTriggerOnUnguidedCal

Set ECal Auto-orient

SENSe:CORRection:PREFerence:ECAL:ORIentation

cal.OrientECALModule

Set ECal Port Map

SENSe:CORRection:PREFerence:ECAL:PMAP

cal.ECALPortMapEx

Set default Cal Type

None

None

 

Port Extensions

Extensions ON|OFF

SENSe:CORRection:EXTension

portExtension.State

Port 1 Extensions Value

SENSe:CORRection:EXTension:PORT

portExt.Port1

Port 2 Extensions Value

SENSe:CORRection:EXTension:PORT

portExt.Port2

Set Freq 1|2

SENSe:CORRection:EXTension:PORT:FREQuency

Fix.PortFreq1

Set Loss 1|2

SENSe:CORRection:EXTension:PORT:LOSS

fix.PortLoss1

Use 1|2

SENSe:CORRection:EXTension:PORT:INCLude

fix.PortExtUse1

Set Loss at DC

SENSe:CORRection:EXTension:PORT:LDC

fix.PortLossDC

Relative Velocity

SENSe:CORRection:RVELocity:COAX

app.VelocityFactor

Port Ext in distance

SENSe:CORRection:EXTension:PORT:DISTance

PortDistance

Set distance units

SENSe:CORRection:EXTension:PORT:UNIT

PortDistanceUnit

Set Media per port

SENSe:CORRection:EXTension:PORT:MEDium

PortMedium

Set waveguide cutoff freq per port

SENSe:CORRection:EXTension:PORT:WGCutoff

PortWGCutoffFreq

Set Velocity Factor per port

SENSe:CORRection:EXTension:PORT:VELFactor

PortVelocityFactor

Couple to system Velocity Factor

SENSe:CORRection:EXTension:PORT:SYSVelocity

PortCoupleToSystemVelocity

Couple to system Media type

SENSe:CORRection:EXTension:PORT:SYSMedia

PortCoupleToSystemMedia

 

Auto Port Extensions

Measure OPEN or SHORT for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:MEASure

AutoPortExtMeasure

Sets the frequencies used for Auto Port Ext. calculation.

SENSe:CORRection:EXTension:AUTO:CONFig

AutoPortExtConfig

Include loss correction in Auto Port Ext.?

SENSe:CORRection:EXTension:AUTO:LOSS

AutoPortExtLoss

Include DC Offset in Auto Port Ext.?

SENSe:CORRection:EXTension:AUTO:DCOFfset

AutoPortExtDCOffset

Enable specified port for Auto Port Ext..

SENSe:CORRection:EXTension:AUTO:PORT<n>

AutoPortExtState

Clears old port extension delay and loss data.

SENSe:CORRection:EXTension:AUTO:RESet

AutoPortExtReset

Set user span start frequency for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:STARt

AutoPortExtSearchStart

Set user span stop frequency for Auto Port Ext.

SENSe:CORRection:EXTension:AUTO:STOP

AutoPortExtSearchStop

 

Fixturing Commands

See also Ground Loop De-embedding/Embedding commands

Turn fixturing ON and OFF

CALCulate:FSIMulator:STATe

FixturingState

Change order of operations

CALCulate:FSIMulator:SENDed:OORDer

None

2and 4-port Extrapolate

CALCulate:FSIMulator:SNP:EXTRapolate

EnableSnPDataExtrapolation

2-Port Fixturing

Port matching ON and OFF

CALCulate:FSIMulator:SENDed:PMCircuit:STATe

PortMatchingState

Reverse ports

CALCulate:FSIMulator:SENDed:DEEMbed:PORT<n>:SNP:REVerse

Reverse2PortAdapter

Sets Port Matching circuit model.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:TYPE

PortMatchingCktModel

Sets Port Matching 'S2P' file name.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:USER:FILename

strPortMatch_S2PFile

Sets Capacitance 'C' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:C

PortMatching_C

Sets Conductance 'G' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:G

PortMatching_G

Sets Inductance 'L' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:L

PortMatching_L

Sets Resistance 'R' value.

CALCulate:FSIMulator:SENDed:PMCircuit:PORT:PARameters:R

PortMatching_R

De-embed ON and OFF

CALCulate:FSIMulator:SENDed:DEEMbed:STATe

Port2PdeembedState

Sets De-embedding circuit model.

CALCulate:FSIMulator:SENDed:DEEMbed:PORT

Port2PdeembedCktModel

Sets De-embedding 'S2P' file name.

CALCulate:FSIMulator:SENDed:DEEMbed:PORT:USER:FILename

strPort2Pdeembed_S2PFile

Port Impedance ON and OFF

CALCulate:FSIMulator:SENDed:ZCONversion:STATe

PortArbzState

Port Z Real

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:REAL

PortArbzReal

Port Z Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:IMAG

PortArbzImag

Port Z Real and Imag

CALCulate:FSIMulator:SENDed:ZCONversion:PORT:Z0

PortArbzZ0

4-Port Network Embed/De-embed commands

Specifies the PNA / DUT topology

CALCulate:FSIMulator:EMBed:TYPE

Embed4PortTopology

Specifies the 4-port touchstone file

CALCulate:FSIMulator:EMBed:NETWork:FILename

Embed4PortNetworkFilename

Embed|De-embed?

CALCulate:FSIMulator:EMBed:NETWork:TYPE

Embed4PortNetworkMode

Specify PNA port connections

CALCulate:FSIMulator:EMBed:TOPology:A:PORTs

CALCulate:FSIMulator:EMBed:TOPology:B:PORTs

CALCulate:FSIMulator:EMBed:TOPology:C:PORTs

CALCulate:FSIMulator:EMBed:TOPology:D:PORTs

Embed4PortList

SetCustomDUTTopology

4-port remap

CALCulate:FSIMulator:EMBed:NETWork<n>:PMAP

NetworkPortMap

Turn ON or OFF

CALCulate:FSIMulator:EMBed:STATe

Embed4PortState

Maps the physical VNA ports to a device of balanced and single-ended logical ports for multi-port systems with greater than 4 ports

CALCulate:DTOPology

SetCustomDUTTopology

Differential Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BALun:DZConversion:BPORT:Z0

DiffZConvPortZ0

Sets real part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORT:REAL

DiffZConvPortReal

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:DZConversion:BPORT:IMAG

DiffZConvPortImag

Turn ON or OFF

CALCulate:FSIMulator:BALun:DZConversion:STATe

DiffZConvState

Common Mode Port Arbitrary Impedance

Sets the impedance value

CALCulate:FSIMulator:BALun:CZConversion:BPORT:Z0

CmnModeZConvPortZ0

Sets real part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORT:REAL

CmnModeZConvPortReal

Sets imaginary part of impedance

CALCulate:FSIMulator:BALun:CZConversion:BPORT:IMAG

CmnModeZConvPortImag

Turn ON or OFF

CALCulate:FSIMulator:BALun:CZConversion:STATe

CmnModeZConvState

Differential Port Matching

Sets type of circuit to embed.

CALCulate:FSIMulator:BALun:DMCircuit:BPORt

DiffPortMatchMode

Specifies the 2-port touchstone file

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:USER:FILename

DiffPortMatchUserFilename

Sets Capacitance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:C

DiffPortMatch_C

Sets Conductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:G

DiffPortMatch_G

Sets Inductance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:L

DiffPortMatch_L

Sets Resistance value

CALCulate:FSIMulator:BALun:DMCircuit:BPORt:PARameters:R

DiffPortMatch_R

Turns ON/OFF

CALCulate:FSIMulator:BALun:DMCircuit:STATe

DiffPortMatchState

Power Compensation

Compensate source power

CALCulate:FSIMulator:SENDed:POWer:PORT:COMPensation

EnablePowerCompensation

Remote ONLY

Create Cal Set with De-embeded fixture removed.

CSET:FIXTure:DEEMbed

Deembed

Create Cal Set with Matching network included.

CSET:FIXTure:EMBed

Embed

 

Cal Plane Manager

SCPI

COM

Characterize a fixture

CSET:FIXTure:CHARacterize

CharacterizeFixture

Creates a single S2P file from two existing files.

CSET:FIXTure:CASCade

CascadeS2PFiles

 

Global Delta Match Cal

Initiate Cal

SENSe:CORRection:COLLect:GUIDed:DMATch

guid.GenerateGlobalDeltaMatchSequence

Read ports that require Cal

SENSe:CORRection:COLLect:GUIDed:DMATch:APPLy:PORTs?

guid.PortsNeedingDeltaMatch

Apply a Cal

SENSe:CORRection:COLLect:GUIDed:DMATch:APPLy

guid.ApplyDeltaMatchFromCalSet

 

Manage and Modify Cal Kits

Set a Cal Kit Active

SENSe:CORRection:COLLect:CKIT

app.CalKitType

Clear all Cal Kits from PNA

SENSe:CORRection:CKIT:CLEar

None

Get a Handle to the Active Cal Kit

None

app.ActiveCalKit

Save All Cal Kits after Modifying

None

app.SaveKits

Load collection of Kits

SENSe:CORRection:CKIT:LOAD

None

Load (Recall) All Cal Kits

None

app.RecallKits

Import a specified kit.

SENSe:CORRection:CKIT:IMPort

None

Restore Cal Kit Default

SENSe:CORRection:COLLect:CKIT:RESet

None

Restore ALL Cal Kits Default

SENSe:CORRection:CKIT:INITialize

None

Build a Hybrid Cal Kit

None

app.BuildHybridKit

Set the Name of a Cal Kit

SENSe:CORRection:COLLect:CKIT:NAME

calKit.Name

Set a description of a Cal Kit

SENSe:CORRection:COLLect:CKIT:DESCription

None

Get the amount of installed kits

SENSe:CORRection:CKIT:COUNt?

None

Set the Port Label of a Cal Kit

None

calKit.Portlabel

Saves a Cal Kit to a file.

SENSe:CORRection:CKIT:EXPort

None

 

Modify TRL Cal Kit

Set reference plane

SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane

None

Set impedance standard

SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance

None

Set LRL auto-characterization

SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar

None

 

Modify Cal Standards

Select a Cal Standard

SENSe:CORRection:COLLect:CKIT:STANdard

calkit.GetCalStandard

Delete a standard

SENSe:CORRection:COLLect:CKIT:STANdard:REMove

None

Change description of a standard

SENSe:CORRection:COLLect:CKIT:STANdard:SDEScription

None

Assign a Class to a Standard

SENSe:CORRection:COLLect:CKIT:ORDer1

calKit.StandardForClass

Set Standard Type

SENSe:CORRection:COLLect:CKIT:STANdard:TYPE

calstd.Type

Add connector family name

SENSe:CORRection:COLLect:CKIT:CONNector:ADD

None

Delete connector family name

SENSe:CORRection:COLLect:CKIT:CONNector:DELete

None

List connector family names used in a Cal Kit

SENSe:CORRection:COLLect:CKIT:CONNector:CATalog?

None

Replace connector family name.

SENSe:CORRection:COLLect:CKIT:CONNector:FNAMe

None

Assign connector family name to a standard

SENSe:CORRection:COLLect:CKIT:CONNector:SNAMe

None

Set Delay

SENSe:CORRection:COLLect:CKIT:STANard:DELay

calstd.Delay

Set Loss

SENSe:CORRection:COLLect:CKIT:STANdard:LOSS

calstd.loss

Set Impedance

SENSe:CORRection:COLLect:CKIT:STANdard:IMPedance

calstd.Z0

Set Max Frequency

SENSe:CORRection:COLLect:CKIT:STANdard:FMAXimum

calstd.MaximumFrequency

Set Min Frequency

SENSe:CORRection:COLLect:CKIT:STANdard:FMINimum

calstd.MinimumFrequency

Set Label

SENSe:CORRection:COLLect:CKIT:STANdard:LABel

calstd.Label

Set Medium (coax | waveguide)

SENSe:CORRection:COLLect:CKIT:STANdard:CHARacter

calstd.Medium

Set Capacitance (C0 to C3)

SENSe:CORRection:COLLect:CKIT:STANdard:C0

calstd.C0

Set Inductance (L0 to L3)

SENSe:CORRection:COLLect:CKIT:STANdard:L0

calstd.L0

Set Arbitrary Impedance (TZReal, TZImag)

SENSe:CORRection:COLLect:CKIT:STANdard:TZReal

calstd.TZReal

 

Modify TRL Cal Kit

Set reference plane

SENSe:CORRection:COLLect:CKIT:TRLoption:RPLane

None

Set impedance standard

SENSe:CORRection:COLLect:CKIT:TRLoption:IMPedance

None

Set LRL auto-characterization

SENSe:CORRection:COLLect:CKIT:TRLoption:LRLChar

None

Real-time Uncertainty

Setup Options

SYSTem:UNCertainty:ETERm:NOIS:ENAB

PortNoiseEnabled

SYSTem:UNCertainty:ETERm:CABLe:REPeat

CableRepeatabilityEnabled

SYSTem:UNCertainty:ETERm:SDEFinitions

StandardDefinitionsEnabled

SYSTem:UNCertainty:POINts:MAXimum

MaximumUncertaintyPoints

 

Noise Characterization

Clear noise data on specified port

SYSTem:UNCertainty:PORT<p>:NOISe:RESet

ResetNoise

Clear noise data on all ports

SYSTem:UNCertainty:PORT:NOISe:RESet

ResetNoiseForAllPorts

Copy noise from a port to all ports

SYSTem:UNCertainty:PORT:NOISe:ALL:COPY

CopyNoiseToAllPorts

Start Noise char

SENSe:CORRection:COLLect:GUIDed:UNCertainty:CHARacterize:NOISe

InitiateNoiseCharacterization

 

Cables Characterization

List cables

SYSTem:UNCertainty:CABLe:CATalog?

Cables Collection

Assign Cable to all ports

SYSTem:UNCertainty:PORT:CABLe:ALL

SelectCableForAllPorts

Assign Cable to specified port

SYSTem:UNCertainty:PORT<p>:CABLe

Cable

Reset repeatability

SYSTem:UNCertainty:CABL:REP:RES

ResetRepeatability

Start Cable char

SENS:CORR:COLL:GUID:UNCertainty:CHAR:CABLe

InitiateCableCharacterization

 

Uncertainty workspace

Load workspace

SYSTem:UNCertainty:LOAD

Recall

Save workspace

SYSTem:UNCertainty:STORe

Save

 

Enabling a Guided Calibration to include Uncertainties

Checkbox on Guided Cal Select Ports page

SENSe:CORRection:COLectL:GUIDed:UNCertainty

UncertaintyEnabled

 

Trace Properties

CALCulate:MEASure:UNCertainty:DISPlay:TYPE

DisplayType

CALCulate:MEASure:UNCertainty:DISPlay:CFACtor

CoverageFactor

CALCulate:MEASure:UNCertainty:MODE:NOISe

MeasurementNoiseUncertainty

CALCulate:MEASure:UNCertainty:MODE:CABLe:REPeat

CableRepeatabilityUncertainty

CALCulate:MEASure:UNCertainty:MODE:ETERm

ErrorTermUncertainty

Apply to all traces

None

None

Add Trace

None

None

Save uncertainty data

CALCulate:MEASure:UNCertainty:SAVE

WriteUncertaintyFile

 

Multiple Power Sensors

 See commands to configure a Power Meter as Receiver (PMAR)

Enable multiple sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple

UseMultipleSensors

Add sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:ADD

Add

Assign power sensor name

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:NAME

Name

Remove sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:REMove

Remove

Read the number of configured sensors

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:COUNt?

Count

Set start freq

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:FREQuency:STARt

StartFrequency

Set stop freq

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:FREQuency:STOP

StopFrequency

Set connector type

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:CONNector

PowerSensorConnectorType

Set Cal Kit

SENSe:CORRection:COLLect:GUIDed:PSENsor:MULTiple:CKIT

PowerSensorCalKitType

 

Source Power Calibration

Copy Source Power cal to another channel

SYSTem:MACRo:COPY:CHANnel:SOURce

ApplySourcePowerCorrectionTo

GPIB Power Meter Address

SYSTem:COMMunicate:GPIB:PMETer:ADDRess

pwrCal.PowerMeterGPIBAddress

Set source power cal method

SOURce:POWer:CORRection:COLLect:ACQ

SetCalInfoEx Method

Turn correction ON|OFF

SOURce:POWer:CORRection

SourcePowerCorrection

Applies correction values after completing a source power cal acquisition sweep.

Optionally do reference receiver cal.

SOURce:POWer:CORRection:COLLect:SAVE

ApplyPowerCorrectionValuesEx

Returns the currently-selected power sensor channel (A or B) for use at a specific frequency.

None

PowerAcquisitionDevice

Set power level

SOURce:POWer:CORRection:LEV

SetCalInfoEx Method

Set power offset

SOURce:POWer:CORRection:OFFSet

SourcePowerCalPowerOffset

Set settling tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

ReadingsTolerance

Set max readings for settling

SOURce:POWer:CORRection:COLLect:AVERerage:COUNt

ReadingsPerPoint

Set accuracy tolerance

SOURce:POWer:CORRection:COLLect:ITERation:NTOLerance

IterationsTolerance

Set max readings for accuracy

SOURce:POWer:CORRection:COLLect:ITERation:COUNt

MaximumIterationsPerPoint

Turn ON|OFF display of readings

SOURce:POWer:CORRection:COLLect:DISPlay

AcquirePowerReadingsEx

Acquire receiver-only readings

SOURce:POWer:CORRection:COLLect:ACQuire:REC

AcquirePowerReadingsEx

Initiates a source power cal acquisition.

SOURce:POWer:CORRection:COLLect:ACQuire

AcquirePowerReadingsEx

Aborts a source power cal acquisition sweep that is currently in progress.

SOURce:POWer:CORRection:COLLect:ABORt

AbortPowerAcquisition

Launches the Configure Power Sensor dialog on the PNA.

None

LaunchPowerMeterSettingsDialog

Frequency checking (ON|OFF)

SOURce:POWer:CORRection:COLLect:FCHeck

UsePowerSensorFrequencyLimits

Check test port power

None

CheckPower

Calibrate the source at multiple power levels.

None

None

Specifies if the source power cal in the calset linked to a measurement cal should be enabled or disabled with that cal

None

PreferSourcePowerCalFromCalset

Enable/disable use of error messages during a source calibration if calibration fails to achieve desired power level at the power sensor

SOURce:POWer:CORRection:COLLect:WARN

None

 

Power Meter/Sensor settings

 See commands to configure a Power Meter as Receiver (PMAR)

 See commands to configure multiple power sensors for guided Power Cal

Specifies the type of power sensor to be used

SYSTem:COMMunicate:PSENsor

Path

Specifies the location of the power sensor to be used.

SYSTem:COMMunicate:PSENsor

Locator

Returns the ID string of connected USB power meters / sensors.

SYSTem:COMMunicate:USB:PMETer:CATalog?

USBPowerMeterCatalog

Pwr meter Max Readings for settling

SOURce:POWer:CORRection:COLLect:AVERerage:COUNt

ReadingsPerPoint

Pwr meter settling tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

ReadingsTolerance

Minimum Frequency

SOURce:POWer:CORRection:COLLect:<>SENsor

MinimumFrequency

Maximum Frequency

SOURce:POWer:CORRection:COLLect:<>SENsor

MaximiumFrequency

Power meter channel

None

PowerMeterChannel

Set sensor cal factor

SOURce:POWer:CORRection:COLLect:<>SENsor:RCFactor

ReferenceCalFactor

Set table type

SOURce:POWer:CORRection:COLLect:TABLe <>SENsor

None

Read/Write cal data

SOURce:POWer:CORRection:DATA

See Data

Use Loss table?

SOURce:POWer:CORRection:COLLect:TABLe:LOSS

UsePowerLossSegments

Cal Factor Table

SOURce:POWer:CORRection:COLLect:TABLe:SELect

CalFactorSegments Collection

Read number of segments in table

SOURce:POWer:CORRection:COLLect:TABLe:POINts?

Count

Segment number

None

SegmentNumber

Add segment

None

Add

Cal factor of the segment

SOURce:POWer:CORRection:COLLect:TABLe:DATA

CalFactor

Frequency of the segment

SOURce:POWer:CORRection:COLLect:TABLe:FREQuency

Frequency

Power Loss Table

SOURce:POWer:CORRection:COLLect:TABLe:SELect

PowerLossSegments Collection

Read number of segments in table

SOURce:POWer:CORRection:COLLect:TABLe:POINts?

Count

Segment number

None

SegmentNumber

Add segment

None

Add

Frequency

SOURce:POWer:CORRection:COLLect:TABLe:FREQuency

Frequency

Loss value

SOURce:POWer:CORRection:COLLect:TABLe:DATA

Loss

Receiver Cal

Set offset from test port power

SENSe:CORRection:RPOWer:OFFSet[:AMPLitude]

DoReceiverPowerCal

Set cal method to receiver cal

SENSe:CORRection:COLLect:METHod RPOWer

DoReceiverPowerCal

Take measurement

SENSe:CORRection:COLLect[:ACQuire] POWer

None

Turn receiver cal ON | OFF

SENSe:CORRection[:STATe] ON|OFF

Error Correction

Do interpolation

SENSe:CORRection:INTerpolate[:STATe] ON|OFF

InterpolateCorrection

 

CalPod

Command used to send other commands as arguments

CONTrol:CALPod:COMMand

None

Start the CalPod software

Calpod:LAUNch

None

Assign Calpod serial number to a port.

Calpod:ENABle

None

Unassign Calpod serial number from a port.

Calpod:Disable

None

Initialize the selected channel

Calpod:INITialize:ACTive

None

Initialize ALL channels

Calpod:INITialize:ALL

None

Recorrect the selected channel

Calpod:Recorrect:ACTive

None

Recorrect ALL channels

Calpod:Recorrect:ALL

None

Show refresh dialog

Calpod:SHOW

None

Hide refresh dialog

Calpod:HIDE

None

Sets impedance state

Calpod:STATe

None

Read Calpod temperature

Calpod:TEMP?

None

 

Custom Cal Window

Turn ON | OFF Custom Cal window.

SENSe:CORRection:COLLect:DISPlay:WINDow

DisplayNAWindowDuringCalAcquisition

Show NO Custom Cal windows.

SENSe:CORRection:COLLect:DISPlay:WINDow:AOFF

DisplayOnlyCalWindowDuringCalAcquisition

Specify channel to sweep before Cal acquisition.

SENSe:CORRection:COLLect:SWEep:CHANnel

AllowChannelToSweepDuringCalAcquisition

Sweep NO channel before Cal acquisition.

SENSe:CORRection:COLLect:SWEep:CHANnel:AOFF

SweepOnlyCalChannelDuringCalAcquisition

Preview sweep before remote Cal acquisition.

SENSe:CORRection:COLLect:GUIDed:PACQuire

SetupMeasurementsForStep

 

Retrieve and Put Calibration Data

Retrieve Cal Data from the PNA

SENSe:CORRection:CSET:DATA

see Data Topic

Put Cal Data in the PNA

SENSe:CORRection:CSET:DATA

see Data Topic

 

Automatic Fixture Removal (AFR)

Turns on or off the option "Automatically iterate when ‘Impedance Method Auto’ is checked."

AFR:ADVanced:AUTO:ITERate:METHod:CHECk[:STATe]  None

Turns on or off the option "Automatically iterate when Calibration Reference Z0 is set to System Z0 or custom value.

AFR:ADVanced:AUTO:ITERate:REFZ:SET[:STATe]  None

Gets or sets the DUT gate coefficient.

AFR:ADVanced:DUTGate:COEFficient None

Sets or gets the description of the AFR DUT Gate Domain (single-ended or differential).

AFR:ADVanced:DUTGate:DOMain None

Turns ON or OFF the Fitting Thru after AFR DUT Gate.

AFR:ADVanced:DUTGate:ILFitting:MANual[:STATe] None

Turns ON or OFF AFR DUTGate

AFR:ADVanced:DUTGate:MANual[:STATe] None

Turns ON or OFF AFR DUTGate Only Reflection Option

AFR:ADVanced:DUTGate:REFLection:MANual[:STATe] None

Applies advanced algorithm to fixture impedance mismatching cases for better results.

AFR:ADVanced:FIXTure:IMPedance:FTUNe[:STATe] None

Turns ON of OFF AFR mode conversion.

AFR:ADVanced:MCONversion[:STATe]

None

Sets or reads the gating mode in 1-port characterization.

AFR:ADVanced:REFLection:GATing:MODE  None
Gets or sets the position parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:MODE::CUSTom:POSition None
Gets or sets the N parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:MODE:MINimum:NVALue None
Gets or sets the spike tolerance parameter in 1-port characterization. AFR:ADVanced:REFLection:GATing:SPIKe:TOLerance None
Gets or sets the ratio of the merge center for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:MCENter None
Gets or sets the ratio of the merge span for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:MSPan None
Gets or sets the start ratio for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:STARt None
Gets or sets the stop ratio for IL fitting at high frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:HIGH:STOP None
Gets or sets the ratio of the merge center for IL fitting at low frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:LOW:MCENter  None

Gets or sets the ratio of the merge span for IL fitting at low frequency range 1-port characterization.

AFR:ADVanced:REFLection:ILFitting:LOW:MSPan None
Gets or sets the start ratio for IL fitting at low frequency range 1-port characterization. AFR:ADVanced:REFLection:ILFitting:LOW:STARt None

Gets or sets the stop ratio for IL fitting at low frequency range 1-port characterization.

AFR:ADVanced:REFLection:ILFitting:LOW:STOP None

Resets the AFR configuration.

AFR:ADVanced:RESet

None

Gets or sets the manual start time in AFR configuration.

AFR:ADVanced:TIME:STARt

None

Gets or sets the manual stop time in AFR configuration.

AFR:ADVanced:TIME:STOP

None

Gets the AFR Version. AFR:ADVanced:VERSion? None

Gets or sets the manual window type in AFR configuration.

AFR:ADVanced:WINDow:COEFficient

None

Turns ON of OFF the manual window coefficient of the AFR.

AFR:ADVanced:WINDow:MANual[:STATe]

None

Selects whether the fixture is band limited or not.

AFR:FIXTure:BLIMited[:STATe]

None

Selects whether to use DUT correction or not when the characterization fixture is not equal to the DUT measurement fixture.

AFR:FIXTure:CDUT[:STATe]

None

Selects Fixture Length A not equal to B correction.

AFR:FIXTure:CLENgth[:STATe]

None

Selects Fixture Match A not equal to B correction.

AFR:FIXTure:CMATch[:STATe]

None

Describes the fixture inputs (single ended or differential).

AFR:FIXTure:INPuts

None

Selects the number of fixtures to be characterized.

AFR:FIXTure:MEASurement

None

Refreshes preview data.

AFR:FIXTure:PREView

None

Reads the impedance profile of the calculated fixture model.

AFR:FIXTure:PREView:DATA[:IMPedance]?

None

Reads the impedance profile of the calculated fixture model at a specified position.

AFR:FIXTure:PREView:DATA[:IMPedance]:MARKer:Y?

None

Chooses the calibration reference Z0 after fixture removal.

AFR:FIXTure:REFZ

None

Sets "System Z0" to Calibration Reference Z0.

AFR:FIXTure:SET:SYSZ[:STATe]

None

Specifies whether thrus are used in case of multi-port fixtures.

AFR:FIXTure:USE:THRUs[:STATe]

None

Restores the default AFR settings.

AFR:INITialize

None

Specifies the file paths of saved fixture data.

AFR:SAVE:FILename

None

Specifies whether the port impedances are normalized in saving the AFR fixture files.

AFR:SAVE:IMPedance:NORMalize[:STATe]

None

Assigns the ports for saved fixture data in several formats.

AFR:SAVE:PORTs

None

Sets the file type to save fixture data.

AFR:SAVE:TYPE

None

Selects all OPEN standards.

AFR:STANdard:ALLOpen[:STATe]

None

Selects all SHORT standards.

AFR:STANdard:ALLShort[:STATe]

None

Reads the impedance profile of the measured standard.

AFR:STANdard:DATA[:IMPedance]?

None

Reads the impedance of the measured standard at a specified position.

AFR:STANdard:DATA[:IMPedance]:MARKer:Y?

None

Sets the fixture length for the selected fixture (for 1X AFR only).

AFR:STANdard:EDIT:FLENgth

None

Sets the gate position for the selected fixture.

AFR:STANdard:EDIT:GATE

None

Sets the impedance for the selected term.

AFR:STANdard:EDIT:IMPedance

None

Sets the impedance method.

AFR:STANdard:EDIT:IMPedance:METHod

None

Loads the calibration standards data from a file.

AFR:STANdard:LOAD

None

Measures calibration standard.

AFR:STANdard:MEASure

None

Specifies fixture thru settings.

AFR:STANdard:THRU

None

Chooses the calibration standards.

AFR:STANdard:USE

None

 

Cal Update

Sets and returns the averaging used to improve noise errors.

SYSTem:CALibrate:CALupdate:AVERage:COUNt

None

Sets and returns the IF bandwidth used by the measurement channel.

SYSTem:CALibrate:CALupdate:BWIDth[:RESolution]

None

Selects the channel(s) to calibrate.

SYSTem:CALibrate:CALupdate:CHANnel[:SELect]

None

Sets and returns the gate start value for time domain gating.

SYSTem:CALibrate:CALupdate:GATE:STARt

None

Sets and returns the state of gate coupling for gate start value.

SYSTem:CALibrate:CALupdate:GATE:STARt:COUPle[:STATe]

None

Sets and returns the gate stop value for time domain gating.

SYSTem:CALibrate:CALupdate:GATE:STOP

None

Sets and returns the state of gate coupling for gate stop value.

SYSTem:CALibrate:CALupdate:GATE:STOP:COUPle[:STATe]

None

Initializes the selected ports.

SYSTem:CALibrate:CALupdate:INITialize

None

Recorrects the list of previously initialized ports.

SYSTem:CALibrate:CALupdate:RECorrect

None

Sets and returns the reference cal set name.

SYSTem:CALibrate:CALupdate:REFerence

None

Selects the port numbers to initialize.

SYSTem:CALibrate:CALupdate:PORTs[:SELect]

None

Use a channel's existing IF BW, Averaging, and Power value settings or enter the values manually.

SYSTem:CALibrate:CALupdate:SETTings:AUTO

None

Manually sets and returns the source power for the active measurement channel.

SYSTem:CALibrate:CALupdate:SOURce:POWer

None