Write / Read |
About Frequency Settings |
Description |
Sets and reads how the center frequency step size is determined. When TRUE, center steps by 5% of span. When FALSE, center steps by STEP:SIZE value. |
VB Syntax |
chan.CenterFrequencyStepSizeMode = value |
Variable |
(Type) - Description |
|
chan |
(object) - A Channel object |
|
value |
(Enum as NAModes) Choose from: 0 - naAUTO -Step size is set automatically. 1 - naMaunal - Step size is set manually using CenterFrequencyStepSize Property. |
Return Type |
Enum |
Default |
1 - naMaunal |
Examples |
chan.CenterFrequencyStepSizeMode = naAUTO 'Write value = chan.CenterFrequencyStepSizeMode 'Read |
C++ Syntax |
HRESULT get_CenterFrequencyStepSizeMode(tagNAModes* pVal); HRESULT put_CenterFrequencyStepSizeMode(tagNAModes pVal); |
Interface |
IChannel25 |