Read-only |
About Gain Compression |
Description |
Read the VNA port number which is connected to the DUT input. Use SetPortMap Method to change the port mapping. |
VB Syntax |
obj.DeviceInputPort |
Variable |
(Type) - Description |
|
obj |
A Converter (object) or A GainCompression (object) or A SweptIMD (object) or An IMSpectrum (object) A NoiseFigure (object) |
Return Type |
Integer |
Default |
1 |
Examples |
inPort = gca.DeviceInputPort 'Read |
C++ Syntax |
HRESULT get_DeviceInputPort(int* pVal) |
Interface |
IGainCompression ISweptIMD IMSpectrum INoiseFigure6 IConverter6 |