Controls the IM Spectrum settings.
|
Dim app as AgilentPNA835x.Application app.CreateCustomMeasurementEx(1, "IMSpectrum", "Output", 1) Dim IMSpec Set IMSpec = app.ActiveChannel.CustomChannelConfiguration |
Example Program Create and Cal a IM Spectrum Measurement
Method |
InterfaceSee History |
Description |
|---|---|---|
|
IIMSpectrum |
Sets limited port mapping |
|
Property |
Interface |
Description |
|
IIMSpectrum |
ON | OFF state of power coupling for F1 and F2. |
|
|
IIMSpectrum |
Read input port map |
|
|
IIMSpectrum |
Read output port map |
|
|
IIMSpectrum |
Fixed tone spacing value. |
|
|
IIMSpectrum2 |
Superseded with LevelingMethod Set Equal Tone Power state. |
|
|
IIMSpectrum |
Frequency of the F1 tone. |
|
|
IIMSpectrum |
Frequency of the F2 tone. |
|
|
IIMSpectrum |
Center frequency of the main tones. |
|
|
IIMSpectrum3 |
Set tone power leveling mode |
|
|
IIMSpectrum |
Resolution Bandwidth for the measurement. |
|
|
IIMSpectrum |
Receiver Center frequency |
|
|
IIMSpectrum |
Receiver frequency span. |
|
|
IIMSpectrum |
Receiver Start frequency. |
|
|
IIMSpectrum |
Receiver Stop frequency. |
|
|
IIMSpectrum2 |
Superseded with LevelingMethod Set power at DUT input or Output |
|
|
IIMSpectrum |
IMD channel number to which the IM Spectrum channel is coupled. |
|
|
IIMSpectrum |
Enables tracking with an IMD channel. |
|
|
IIMSpectrum |
Step sweep mode for the IM Spectrum channel. |
|
|
IIMSpectrum |
IMD data point number at which the IM spectrum measurement occurs. |
|
|
IIMSpectrum |
IM product to view when SweepType = NTH is specified. |
|
|
IIMSpectrum |
Type of sweep for an IMSpectrum measurement. |
|
|
IIMSpectrum |
Power level of the Main Tones |
|
Interface |
Introduced with VNA Rev: |
|
IIMSpectrum |
8.35 |
|
IIMSpectrum2 |
9.40 |