Read-only |
About Gain Compression |
Description |
Read the VNA port number which is connected to the DUT Output. Use SetPortMap Method to change the port mapping. |
VB Syntax |
obj.DeviceOutputPort |
Variable |
(Type) - Description |
|
obj |
A Converter (object) or A GainCompression (object) or A SweptIMD (object) or An IMSpectrum (object) A NoiseFigure (object) |
Return Type |
Integer |
Default |
2 |
Examples |
outPort = gca.DeviceOutputPort 'Read |
C++ Syntax |
HRESULT get_DeviceOutputPort(int* pVal) |
Interface |
IGainCompression ISweptIMD IMSpectrum INoiseFigure6 IConverter6 |