Write/Read |
About Equal Tone Power |
Description |
Note: This command is replaced with LevelingMethod Property Sets and returns the ON | OFF state of Equal Tone Power for the Swept IMD or IMSpectrum measurement. |
VB Syntax |
object.EqualTonePower = value |
Variable |
(Type) - Description |
|
object |
A SweptIMD or IMSpectrum Object |
|
value |
(Boolean) - Choose from: True - Set equal tone power. False - Do NOT set equal tone power. |
Return Type |
Boolean |
Default |
False |
Examples |
ims.EqualTonePower = true 'Write |
|
value = imd.EqualTonePower 'Read |
|
C++ Syntax |
HRESULT get_EqualTonePower(VARIANT_BOOL* val) HRESULT put_EqualTonePower(VARIANT_BOOL val) |
Interface |
ISweptIMD2 IIMSpectrum2 |