Write/Read |
About Power Leveling |
Description |
Sets and returns the tone power leveling mode. |
VB Syntax |
object.LevelingMethod = value |
Variable |
(Type) - Description |
|
object |
One of the following: |
|
value |
(enum NAIMDLevelMethod) - Choose from: 0 - naNOLevel 1 - naLevelInput 2 - naEqualizeOutput 3 - naLevelOutput |
Return Type |
Enum |
Default |
naNOLevel |
Examples |
imd.LevelingMethod = naEqualizeOutput 'Write |
|
levMode = ims.LevelingMethod 'Read |
|
C++ Syntax |
HRESULT get_LevelingMethod(tagNALevelingMethods* pVal) HRESULT put_LevelingMethod(tagNALevelingMethods newVal) |
Interface |
IIMSpectrum ISweptIMD |