Write/Read |
About Trigger |
Description |
Sets and reads the trigger delay for all measurements in the CHANNEL. This delay is only applied while in app.Source = naTriggerSourceExternal and trigsetup.Scope = naChannelTrigger . After an external trigger is applied, the start of the sweep is delayed for the specified delay value plus any inherent latency. To apply a trigger delay for all channels (Global), use TriggerDelay Property. |
VB Syntax |
chan.ExternalTriggerDelay = value |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
value |
Double- Trigger delay value in seconds. Range is from 0 to 3 seconds. |
Return Type |
Double |
Default |
0 |
Examples |
chan.ExternalTriggerDelay = .003 'Write |
|
delay = chan.ExternalTriggerDelay 'Read |
|
C++ Syntax |
HRESULT get_ExternalTriggerDelay(double *delay); HRESULT put_ExternalTriggerDelay(double delay) |
Interface |
IChannel6 |