Write/Read |
About Trigger |
Description |
Sets and reads the trigger delay for all measurements (GLOBAL). This delay is only applied while in app.Source = naTriggerSourceExternal and trigsetup.Scope = naGlobalTrigger . After an external trigger is applied, the start of the sweep is delayed for the specified delay value plus any inherent latency. To apply a trigger delay for a channel only, use ExternalTriggerDelay Property. |
VB Syntax |
app.TriggerDelay = value |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
value |
Double- Trigger delay value in seconds. Range is from 0 to 3. |
Return Type |
Double |
Default |
0 |
Examples |
app.TriggerDelay = .003 'Write |
|
delay = app.TriggerDelay 'Read |
|
C++ Syntax |
HRESULT get_TriggerDelay(double *delay); HRESULT put_TriggerDelay(double delay) |
Interface |
IApplication |