Write/Read |
About Receiver Cal |
Description |
Note: This property is replaced by DoReceiverPowerCal Method. For Receiver Calibration - Sets or returns the value to offset the normalized unratioed power measurement data. The unratioed power measurement is effectively calibrated to the power level specified by the value of LogMagnitudeOffset as soon as the Normalization property is set to ON after calling the DataToDivisor method. To offset the data trace magnitude a specified value, use MagnitudeOffset Property |
VB Syntax |
meas.LogMagnitudeOffset = value |
Variable |
(Type) - Description |
|
meas |
(object) - A Measurement object |
|
value |
(double) - Offset value in dBm. |
Return Type |
Double |
Default |
0 |
Examples |
meas.LogMagnitudeOffset = -10 'Write (-10 dBm) |
|
calpower = meas.LogMagnitudeOffset 'Read |
|
C++ Syntax |
HRESULT put_LogMagnitudeOffset(double newVal); HRESULT get_LogMagnitudeOffset(double *pVal); |
Interface |
IMeasurement |