Write/Read |
About IM Spectrum |
Description |
Sets and returns the receiver Center frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
VB Syntax |
ims.SpectrumCenterFrequency = value |
Variable |
(Type) - Description |
|
ims |
An IMSpectrum Object |
|
value |
(Double) Center frequency in Hz. Choose a frequency within the range of the VNA. |
Return Type |
Double |
Default |
1.0 GHz |
Examples |
ims.SpectrumCenterFrequency = 10e9 'Write |
|
value = ims.SpectrumCenterFrequency 'Read |
|
C++ Syntax |
HRESULT get_SpectrumCenterFrequency(double *pVal) |
Interface |
IIMSpectrum |