Write/Read |
About IM Spectrum |
Description |
Sets and returns the receiver Stop frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
VB Syntax |
ims.SpectrumStopFrequency = value |
Variable |
(Type) - Description |
|
ims |
An IMSpectrum Object |
|
value |
(Double) Stop frequency in Hz. Choose a frequency within the range of the VNA. |
Return Type |
Double |
Default |
950 MHz |
Examples |
ims.SpectrumStopFrequency = 10e9 'Write |
|
value = ims.SpectrumStopFrequency 'Read |
|
C++ Syntax |
HRESULT get_SpectrumStopFrequency(double *pVal) |
Interface |
IIMSpectrum |