Write/Read |
About Tone Power |
Description |
Note: This command is replaced with LevelingMethod Property Sets and returns whether tone power is specified at the DUT input or output. |
VB Syntax |
object.TonePowerSetAt = value |
Variable |
(Type) - Description |
|
object |
A SweptIMD Object or IMSpectrum Object |
|
value |
(Enum as NAPortMode) 0 - naInput - Specified power level is set at the DUT input. 1 - naOutput - Specified power level is set at the DUT output. |
Return Type |
Enum |
Default |
0 - naInput |
Examples |
imd.TonePowerSetAt = naOutput 'Write |
|
value = ims.TonePowerSetAt 'Read |
|
C++ Syntax |
HRESULT get_TonePowerSetAt(tagNAPortMode *pVal) HRESULT put_TonePowerSetAt(tagNAPortMode pVal) |
Interface |
ISweptIMD2 IImSpectrum2 |