Write/Read |
About IM Spectrum |
Description |
When an IMD channel exists, allows the IM Spectrum frequency and power setting to track (couple with) the IMD channel settings. Use TrackingChannel to set the channel number to track. |
VB Syntax |
ims.TrackingEnable = value |
Variable |
(Type) - Description |
|
ims |
An IMSpectrum Object |
|
value |
(Boolean) Tracking state. Choose from: True - IM Spectrum frequency and power settings track the IMD channel settings. False - IM Spectrum frequency and power settings are specified in the IMS channel. |
Return Type |
Boolean |
Default |
False |
Examples |
ims.TrackingEnable = True 'Write |
|
value = ims.TrackingEnable 'Read |
|
C++ Syntax |
HRESULT get_TrackingEnable(VARIANT_BOOL* bValue) |
Interface |
IIMSpectrum |