Write/Read |
About IM Spectrum |
Description |
When TrackingManualStepEnable = True (Manual step), sets and returns the data point number at which the IM spectrum measurement occurs. |
VB Syntax |
ims.TrackingStepIndex = value |
Variable |
(Type) - Description |
|
ims |
An IMSpectrum Object |
|
value |
(Integer) Existing IMD channel number to which frequency and power settings are coupled. |
Return Type |
Long Integer |
Default |
1 |
Examples |
ims.TrackingStepIndex = 50 'Write |
|
value = ims.TrackingStepIndex 'Read |
|
C++ Syntax |
HRESULT get_TrackingStepIndex(long *pVal) |
Interface |
IIMSpectrum |