Controls two output functions: RF power and Noise Source.
OUTPut: | [:STATe] |
Click on a red keyword to view the command details.
See Also
Applicable Models: All without M937xA and P93xxA/B (Read-Write) Sets and reads the noise source (28V) ON or OFF. Note: “usbNsSrcID” is an optional parameter. If this optional parameter is specified, it turns the noise source on/off for the specified devices. |
|
Parameters |
|
<bool> |
ON (1) - Noise source ON OFF (0) - Noise source OFF |
Examples |
OUTP:MAN:NOIS
"U1832A MY12345678",1 |
Query Syntax |
OUTPut:MANual:NOISe[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
For VNA models with a Noise Figure option (028/029/H29), the 28V line is always ON. The ON/OFF state is also available from a VNA softkey menu. For VNA models WITHOUT a Noise Figure option (028/029/H29), the 28V line is OFF by default and survives a preset. The ON/OFF state is NOT available from a VNA softkey menu. |
|
Applicable Models: All (Read-Write) Turns RF power from the source ON or OFF. See note about source power state with instrument state save and recall. |
|
Parameters |
|
<ON | OFF> |
ON (or 1) - turns RF power ON OFF (or 0) - turns RF power OFF |
Examples |
OUTP
ON |
Query Syntax |
OUTPut[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|