PNA-X and N522xB Rear Panel


See Differences between the PNA-X and N522xB Models

See N523xB rear-panel.

See NA520xA PNA-X Pro rear panel

Click image to learn more.

 


CPU Version 9.0

 


CPU Version 7.0/8.0/9.0 Connector Reference

The following table shows the connectors for CPU versions 7.0, 8.0, and 9.0:

Connector Name

CPU 7.0, 8.0

CPU 9.0

VGA

Yes

No

Display Port Mini

Yes

No

Display Port

No

Yes

1GB LAN

Yes

Yes

10GB LAN

No

Yes

GPIB

Yes

Yes

USB3 (rear panel)

2 Ports

4 Ports

USB2 (rear panel)

1 Port

0 Ports

USB-B 3.0 Device Side

Yes

Yes

USB-C (USB 3.1/Thunderbolt)

No

Yes

PCIe

Yes

No

SATA 2.5 SSD

Yes

No

NVMe SSD

No

Yes


10 MHz Reference IN/OUT

10 MHz Reference Input  When a 10 MHz external reference signal is detected at this port, it will be used as the instrument frequency reference instead of the internal frequency reference.

10 MHz Reference Output  This BNC(f) connector outputs a frequency reference signal for use by other test equipment.

See Specifications

See Reference


Line Power

See Specifications


SRC3 Connector

Provides a synthesizer output from 10 MHz to 13.5 GHz (Option XSB) and also requires Option 422 or 423.

GPIB Controller and Talker/Listener Ports

The PNA-X can be a GPIB Controller and Talker/Listener. Learn more.


PCIe X4 Connector (CPU 8.0, 7.0)

The PCIe X4 connector is a 4-lane slot for future enhancements.


USB Hub

This USB hub contains two SuperSpeed USB ports to power your VNA peripherals. There is also one USB port below the LAN connector, one USB device port, and four USB ports on the front panel.

Limitation: The total current limit for all rear panel USB ports is 2.3 amps. The total current limit for all front panel USB ports is 2 amps. When first connected, Keysight ECal modules 8509x and N4431 draw significantly more current than other modules. See Specifications.

PNA with CPU Version 9.0

This USB hub contains four SuperSpeed USB ports to power your VNA peripherals. There is also one USB device port, and four USB ports on the front panel. The CPU 9.0 provides a total current limit on the four USB-3.0 ports of 3.6 amps.

 

See Important First-time USB connection note.


Display Port (CPU 9.0)

The Display Port is used to connect to external displays and replaces the VGA connector.


USB Device  Learn more


USB-C Connectors (CPU 9.0)

Two USB-C connectors with support for:

1(high power devices require external power supply)


1G LAN Connector (CPU 9.0)

Gigabit Ethernet port supports speeds up to 1 Gb/s.


10G LAN Connector (CPU 9.0)

Gigabit Ethernet port supports speeds up to 10 Gb/s1.

1Wake on LAN not supported on 10G LAN.


LAN Connector

This 10/100/1000 BaseT Ethernet connection has a standard 8-pin configuration and auto selects between the data rates.


Mini DisplayPort Connector (CPU 8.0, 7.0)

The Mini DisplayPort is a miniature DisplayPort connector for connection to external displays.


VGA Connector (CPU 8.0, 7.0)  Learn more


Solid State Drive (SSD) (CPU 8.0, 7.0)

See Service Guide to learn how to remove the SSD. (Internet connection required)

See Preventing VNA SSD Problems


NVMe Solid State Drive (SSD) (CPU 9.0)

Non-Volatile Memory Express solid state drive.

See Service Guide to learn how to remove the SSD. (Internet connection required)

See Preventing VNA SSD Problems


RF Path Access

These connectors are NOT available on the N522x and N5264B models.

These connectors allow RF Path Configuration.

Ports 3 and 4 are not available on 2-port models.

N5247A - J8 thru J11 are moved to the front-panel.


RF and LO OUT

The RF OUT connector is NOT available on the N5264B

For the N5247B and N5227B:- Added RF2 OUT (J12) for 4-port 110 GHz single sweep VNA. Enables driving two mmWave modules  simultaneously. Learn more.

Caution:  LO OUT has more power than previous VNA models.

See specifications


IF Path Inputs

Option 020 adds these connectors, which allow access to the VNA Receiver / IF paths.

These are labeled A, B, C/R1, D/R2, R.

See IF Path Configuration settings and block diagram.


Power I/O

See Details


+28 VDC (BNC output)

Used to power a noise source for the Noise Figure App.


External and AUX Trigger I/O

MEAS TRIG IN - When enabled, VNA is triggered by signals on this connector. Learn more.

MEAS TRIG RDY  When enabled, VNA outputs a 'READY' signal on this connector to other devices. Learn more.

AUX TRIG 1&2 IN  When enabled, VNA accepts signals on these connectors which indicates that the external devices are ready to be triggered. Learn more.

AUX TRIG 1&2 OUT  When enabled, VNA outputs signals on these connectors either before or after a measurement. Learn more.

Test Set I/O

See Details


Bias IN and Fuses

Connect your DC Power Supply to apply Bias to the VNA ports through these BNC connectors.


Material Handler I/O

See details.


Pulse I/O

See Details


CPU

See CPU Speed / Performance

See Determine Your VNA's CPU Version (Internet connection required)