This command is superseded by the SOURce:POWer:ATTenuation:RECeiver:TEST command.
Learn about Receiver Attenuation
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets the attenuation level for the specified receiver. Note: Attenuation cannot be set with Sweep Type set to Power Note: For M980xA/P50xxA/E5080B Receiver Gain, use :SENS:SOUR:REC:GAIN. |
|
Parameters |
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
<recvr> |
Receiver to get attenuation. Choose from:
Receiver attenuation can NOT be set using logical receiver notation. |
<num> |
Attenuation value in dB. To determine how many receiver attenuators, the maximum receiver attenuation, and attenuation step size, for a VNA model, see VNA Models and Options. If a number other than these is entered, the analyzer will select the next lower valid value. For example, if 19 is entered for the E8361A/C, then 10 dB attenuation will be selected. |
Examples |
SENS:POW:ATT
AREC,10 |
Query Syntax |
SENSe<cnum>:POWer:ATTenuator? <rec> |
Return Type |
Numeric |
0 |
|