This program adjusts the Option 205 (2-port) or Option 425 (4-port) Low Frequency Extension (LFE) receivers for a flat response across the full frequency range. The range of this adjustment is 500 Hz to 210 MHz. Learn more about LFE.
This adjustment is for service only; not for measurement calibration.
See list of supported power meters and sensors.
See VNA Accessories
Notes
|
Click Utility, then System, then Service, then Adjustment Routines...
At
the Adjustments selection, click LFE
Receiver Adjustment. The LFE
Mixer Cal Adjustment dialog
is displayed as shown below.

Select the calibration method (ECal or Mechanical Standards).
Select the power sensor.
Click on the Begin button and follow the instructions displayed in the program.
Follow the instructions displayed in the program.
The correction data is stored in the flash memory.