:CHANnel Subsystem

The Channel subsystem commands control all vertical (Y axis) functions. To control differential waveforms, use the :DIFF Subsystem subsystem.

The commands in the :CHANnel subsystem, as well as a few other Infiniium 2026 commands, include a reference (:CHANnel{N}) that identifies the channel to which the command applies as shown in the following table. For example, you can display connection 1 channel 1 with any of the following four identical commands. (Notice channel identifier highlighted in red.)

:CHAN1:DISPlay ON;
:CHAN1_1:DISPlay ON;
:CHANnel1:DISPlay ON;
:CHANnel1_1:DISPlay ON;
Varieties of the Channel Command
  Channel
1 2 … 7 8
Connection 1 :CHAN1
:CHAN1_1
:CHANnel1
:CHANnel1_1
:CHAN2
:CHAN1_2
:CHANnel2
:CHANnel1_2
  :CHAN7
:CHAN1_7
:CHANnel7
:CHANnel1_7
:CHAN8
:CHAN1_8A
:CHANnel8
:CHANnel1_8
2 :CHAN2_1
:CHANnel2_1
:CHAN2_2
:CHANnel2_2
  :CHAN2_7
:CHANnel2_7
:CHAN2_8
:CHANnel2_8
…          
7 :CHAN7_1
:CHANnel7_1
:CHAN7_2
:CHANnel7_2
  :CHAN7_7
:CHANnel7_7
:CHAN7_8
:CHANnel7_8
8 :CHAN8_1
:CHANnel8_1
:CHAN8_2
:CHANnel8_2
  :CHAN8_7
:CHANnel8_7
:CHAN8_8
:CHANnel8_8

To simplify the documentation of these commands, the channel identification portion each of these commands will be represented by {N} as shown here:

CHANnel{N}:BANDwidth