:CMODe:DISPlay
Command Syntax
:CMODeN:DISPlay {ON | OFF | 1 | 0}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:DISPlay?
Description
Turns the display of the specified common-mode waveform on or off. Use the :CMODe:STATus? command to determine if a common-mode waveform is available for display.
Example
:CMODe5_3:DISPlay ON