:CMODe:PATTern:KPATtern
Command Syntax
:CMODeN:PATTern:KPATtern {OZERo | PRBS7 | EPRBs7 | PRBS9 | EPRBs9
| PRBS11 | EPRBs11 | PRBS13 | EPRBs13 | PRBS15 | EPRBs15 | LPAM4 | JPA
| JPB | JPC | QSSPr | PRBQ9 | PRBQ13 | K28P5 | SSPR | PCIE}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:PATTern:KPATtern?
Description
When you have chosen "selecting from a known pattern" to identify the data signal pattern (see :CMODe:PATTern:MODE), this command lets you select the known pattern:
OZERo— One - ZeroPRBS7— PRBS-7 (127 symbols)EPRBs7— PRBS-7 (128 symbols)PRBS9— PRBS-9 (511 symbols)EPRBs9— PRBS-9 (512 symbols)PRBS11— PRBS-11 (2047 symbols)EPRBs11— PRBS-11 (2048 symbols)PRBS13— PRBS-13 (8191 symbols)EPRBs13— PRBS-13 (8192 symbols)PRBS15— PRBS-15 (32767 symbols)EPRBs15— PRBS-15 (32768 symbols)LPAM4— Linearity (160 symbols)JPA— JP0{0}A (2 symbols)JPB— JP0{0}B (62 symbols)JPC— JP0{0}C (62 symbols)QSSPr— SSPRQ (65535 symbols)PRBQ9— PRBS9Q (511 symbols)PRBQ13— PRBS13Q (8191 symbols)K28P5— K28.5 (20 symbols)SSPR— SSPR (32762 symbols)PCIE— PCIe (8768 symbols)