:DISK:EYE:FNAMe:USTandard

Command Syntax

:DISK:EYE:FNAMe:USTandard

Description

Resets the file name for the colorgrade-grayscale file from using a custom name to using the standard name in the following form:

cg-gs_<date><autonumber>.<extension>

For example, cg-gs_2020-10-23_1.cgsx. Refer to :DISK:EYE:FNAMe to learn about standard and custom names.