:DISK:EYE:SAVE
Command Syntax
:DISK:EYE:SAVE
Description
Saves a color-grade gray-scale waveform to a file. Use the :DISK:EYE:FNAMe command to specify the file name and the :DISK:EYE:SAVE:FTYPe command to specify the file type (.cgsi or .csv). Specify the source waveform using the :DISK:EYE:SAVE:SOURce command. If you want to return the color-grade gray-scale format directly to the computer without Infiniium saving a file, use the :WAVeform:CGRade:XML:READ? and :WAVeform:CGRade:XML:WRITe? commands.
To load a color grade-gray scale file into one of Infiniium's eight color grade memories using the :CGMemory:FILE:LOAD and :CGMemory:FILE:NAME commands.
Example Command Sequence
:DISK:EYE:SAVE:FTYPe DATabase :DISK:EYE:FNAMe "%USER_DATA_DIR%\Colorgrade-Grayscale\myfile" :DISK:EYE:SAVE
Related Commands
:DISK:EYE:FNAMespecifies the saved file's name.:DISK:EYE:FNAMeupdates autonumber, if used.:DISK:EYE:FNAMeresets to the standard file name.:DISK:EYE:SAVE:FTYPespecifies the type of file saved.:DISK:EYE:SAVE:SOURcespecifies the source waveform on which to perform the measurement.