:DISPlay:DIALog:BTRansparent
Command Syntax
:DISPlay:DIALog:BTRansparent {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:DIALog:BTRansparent?
Query Response
{1 | 0}
Description
Turns the ability to display dialog boxes with transparent backgrounds on and off. The default setting is OFF. Use the :DISPlay:DIALog:OPACity command to adjust the level of opacity.