:DISPlay:DIALog:OPACity

Command Syntax

:DISPlay:DIALog:OPACity  <percent>

<percent> is an int.

Query Syntax

:DISPlay:DIALog:OPACity?

Description

Sets the level of a dialog box's background opacity when dialog box transparency is turned on. The opacity can be any value between 0% (clear background) and 100% (solid background). The default setting is 100%. Use the :DISPlay:DIALog:BTRansparent command to turn dialog box transparency on.