:DISPlay:WINDow:FDLegend

Command Syntax

:DISPlay:WINDow:FDLegend {OFF | ON}

Query Syntax

:DISPlay:WINDow:FDLegend?

Description

Shows or hides the Signals identification legend on all frequency-domain windows. This label is displayed in the content window's upper-right corner. The legend identifies:

  • The output of the FFT function in Decibels (Hz), Degrees (Hz), and Seconds (Hz) content windows.