:DISPlay:WINDow:TIME{N}:LEGend:ECEXpand

Command Syntax

:DISPlay:WINDow:TIMEN:LEGend:ECEXpand {ON | OFF}

Where N indicates one of four possible Waveform windows. For example, TIME1.

Query Syntax

:DISPlay:WINDow:TIMEN:LEGend:ECEXpand?

Description

Expands or contracts all displayed Eye Contours legends that are shown in the Waveformcontent window. To display or hide the Eye Contours legend, use the :DISPlay:WINDow:ECLegend command. Use the Eye Contour Configuration Commands to create and display contour lines. If Option 200, Enhanced Jitter Analysis, is also installed, the application leverages the oscilloscope's ability to measure ultra-low levels of Random Jitter (RJ). This can be used to obtain fixed RJ values.

Sibling Commands