:DISPlay:WINDow:TIME{N}:LEGend:EXPand

Command Syntax

:DISPlay:WINDow:TIMEN:LEGend:EXPand {ON | OFF}

Where N indicates one of four possible Waveform windows. For example, TIME1.

Query Syntax

:DISPlay:WINDow:TIMEN:LEGend:EXPand?

Description

Expands or contracts the Signals legend that is shown in the Waveform content window legend. Use the :DISPlay:WINDow:TDLegend command to show or hide the legend on all time-domain windows.

Sibling Commands