:FUNCtion:PARameters:DDEMbed:BSPan?

Query Syntax

:FUNCtionN:PARameters:DDEMbed:BSPan?

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Response

<frequency_span> is a double.

Description

When the BANDpass filter type is selected (see :FUNCtion:PARameters:DDEMbed:BLIMit), this query returns the span of the bandpass filter.