:FUNCtion:PARameters:DDEMbed:IMPulse

Command Syntax

:FUNCtionN:PARameters:DDEMbed:IMPulse {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:DDEMbed:IMPulse?

Query Response

{1 | 0}

Description

For an 4-Port DeEmbedding operator (:FUNCtion:FOPerator), this command turns on and off the Show Impulse Response option. When selected (on), the selected network file is automatically loaded into the S-Parameter/Transfer Function Viewer and an impulse response chart is added if the parameters can be determined; otherwise, you can add the chart by selecting the proper parameters. See :NETWorks:TRACe General Commands.