:FUNCtion:PARameters:DEPort:DRESult

Command Syntax

:FUNCtionN:PARameters:DEPort:DRESult {DSRC | CMSRc}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DEPort:DRESult?

Description

Selects the output type of a 4-Port, 1 Source DeEmbedding operator (:FUNCtion:FOPerator).

The a 4-Port, 1 Source DeEmbedding operator is for situations where the differential or common-mode signal is created prior to de-embedding.

Use the :FUNCtion:PARameters:DEPort:BANDwidth command to specify the function's bandwidth. Use the :FUNCtion:PARameters:DEPort:BLIMit command to specify a bandwidth filter. Use the :FUNCtion:PARameters:DEPort:FNAMe command to open an existing network file that models your test setup.

DSRC
Extracts the differential path from a 4-port transfer function.
CMSRc
Extracts the common-mode path from a 4-port transfer function.

Example Command Sequence

:FUNCtion2:FOPerator DEPort
:FUNCtion2:PARameters:DEPort:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\De-Embedding Networks\DUT_4.tf4"
:FUNCtion2:PARameters:DEPort:DRESult DSRC
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.

Child Commands