:FUNCtion:PARameters:GAUSsian:RTIMe

Command Syntax

:FUNCtionN:PARameters:GAUSsian:RTIMe <rise_time>
            

<rise_time> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:GAUSsian:RTIMe?

Description

Specifies the rise time in seconds of a Gaussian filter operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator GAUSsian
:FUNCtion2:PARameters:GAUSsian:BANDwidth 7.5E6
:FUNCtion2:PARameters:GAUSsian:RTIMe 52.4E-12
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…
                  //  Your code to synchronize execution timing.