:FUNCtion:PARameters:GAUSsian:TFUNction
Command Syntax
:FUNCtionN:PARameters:GAUSsian:TFUNction {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtion{1:64}:PARameters:GAUSsian:TFUNction?
Query Response
{1 | 0}
Description
For the Gaussian filter operator (:FUNCtion:FOPerator), this command turns on and off the Show Transfer Function option. When selected (on), the network is automatically loaded into the S-Parameter/Transfer Function Viewer and a frequency-magnitude chart is added.