:FUNCtion:PARameters:QUSer:CFILe:RELoad
Command Syntax
:FUNCtionN:PARameters:QUSer:CFILe:RELoad
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Reloads the XML configuration file for the selected user-defined function.
Use the :FUNCtion:PARameters:QUSer:CFILe parent command to configure the function.