:FUNCtion:PARameters:QUSer:CFLoaded?
Query Syntax
:FUNCtionN:PARameters:QUSer:CFLoaded?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
{1 | 0}
Description
Queries the existence of the specified user-defined operator. Returns a one if the operator is defined and a zero it the operator has not been setup.
Use the :FUNCtion:PARameters:QUSer:CFILe sibling command to configure the function.