:FUNCtion:PARameters:SINC:BANDwidth
Command Syntax
:FUNCtionN:PARameters:SINC:BANDwidth <cutoff_frequency>
<cutoff_frequency> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtion:PARameters:SINC:BANDwidth?
Description
Specifies the cutoff frequency in Hertz of a Sin(x)/x, or sinc(x), operator (:FUNCtion:FOPerator).