:FUNCtion:PARameters:SINC:STEP

Command Syntax

:FUNCtionN:PARameters:SINC:STEP {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:SINC:STEP?

Query Response

{1 | 0}

Description

For the Sin(x)/x, or sinc(x), operator (:FUNCtion:FOPerator), this command turns on and off the Show Step Response option. When selected (on), the network is automatically loaded into the S-Parameter/Transfer Function Viewer and a step response chart is added.