:LTESt:LLINe:SSUMmary:FNAMe
Command Syntax
:LTESt:LLINe:SSUMmary:FNAMe "<path substitution string>\subfolder\filename"
Where:
- "<path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
- "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Limit Summaries.
- "filename" is a string without the filename extension.
Query Syntax
:LTESt:LLINe:SSUMmary:FNAMe?
Description
Specifies a summary file (file name and path) for limit testing of a limit line test. To enable the saving of summary files, use the :LTESt:LLINe:SSUMmary:STATe command.
Default User Folder
The default folder for storing summary files is in %USER_DATA_DIR%\Limit Summaries as shown in this picture. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Limit Summaries\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Default.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.
A file name must be entered. If an empty string is entered, the writing of the summary file will fail.