:LTESt:MTESt:SIMage:INVert

Command Syntax

:LTESt:MTESt:SIMage:INVert {ON | OFF | 1 | 0}

Query Syntax

:LTESt:MTESt:SIMage:INVert?

Query Response

{1 | 0}

Description

Turns on and off the inversion of the graticule area's background color when reporting a screen capture for a mask limit test. When on, an inverted image will be captured and saved into a file by the :LTESt:MTESt:SIMage:FNAMe command. The entire application window is saved with the graticule black upon a white background. The waveform colors remain unchanged. When printing a hard copy of the waveform, combined this combine with the :LTESt:MTESt:SIMage:WINDow command (graticule only) to save ink or toner. Use the :LTESt:MTESt:SIMage:FNAMe command to enable and disable screen-capture reporting. To enable or disable mask limit tests, use the :LTESt:MTESt:MRESult{N}:STATe command.