:LTESt:MTESt:SIMage:SINClude

Command Syntax

:LTESt:MTESt:SIMage:SINClude {ALL | CHANnel{N} | FUNCtion{1:64} | WMEMory{1:8} | CGMemroy{1:8}}

{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:LTESt:MTESt:SIMage:SINClude?

Description

Selects all or only one of the displayed waveforms to be included on a saved image file when reporting a screen capture for a mask limit test. By default, all waveforms visible on the display are saved in the screen capture. However, when you select one waveform, all other waveform's will be hidden except for their ground markers ( ), which are shown on the screen's right side. Including these markers serves as a reminder that other waveforms were present on the display. Use the :LTESt:MTESt:SIMage:FNAMe command to enable and disable screen-capture reporting. To enable or disable mask limit tests, use the :LTESt:MTESt:MRESult{N}:STATe command.