:MEASure:CLOCk:DCDCycle
Command Syntax
:MEASure:CLOCk:DCDCycle
Query Syntax
:MEASure:CLOCk:DCDCycle?
Description
This command moves the Duty Cycle - Duty Cycle measurement to the top of the Results table and displays the measurement if it is not already shown on the table.
The query form of the command returns the measured value.
The Duty Cycle - Duty Cycle measurement measures the positive pulse width and period of each cycle of the waveform and calculates the duty cycle using the following equation.
The duty cycle of the second cycle of the waveform is found and the first duty cycle is subtracted from the second duty cycle for the first measurement result. Then, the second cycle of the waveform is measured and subtracted from the third cycle duty cycle for the second measurement result. This operation continues until all of the cycles of the waveform have been measured. All of the measurement results are used to compute the statistics. The statistics are the values accumulated over all of the trigger cycles that have occurred.
Use :MEASure:CLOCk:DCDCycle:REGion to specify the waveform data region over which the measurement is made.
Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1_1, WMEMory1, or FUNCtion1.
Use :MEASure:TBASe:GENeral:METHod to change the definition of the waveform's top/base. Use :<waveform>:THReshold:GENeral:METHod to change the definition of the waveform's threshold.
Example Command Sequence
:MEASure:CLOCk:DCDCycle:SOURce CHAN1_1 :MEASure:CLOCk:DCDCycle:EDIRection RISing :MEASure:CLOCk:DCDCycle :MEASure:CLOCk:DCDCycle?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Infiniium.query(':MEASure:CLOCk:DCDCycle:STATus?')):
measurement = Infiniium.query(':MEASure:CLOCk:DCDCycle?')
If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Infiniium.query(':MEASure:CLOCk:DCDCycle:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
measurement = Infiniium.query(':MEASure:CLOCk:DCDCycle?')
You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Querying Measurement Results and Statistics
You can query measurement results using the :MEASure:CLOCk:DCDCycle? query after making the proper instance settings.
If a measurement is installed into Results table (using the :MEASure:CLOCk:DCDCycle command) and you have made the proper instance settings, you can query statistics using common child queries.
Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.